No Qmake in Yocto Build for fsl-image-qt5-validation-imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No Qmake in Yocto Build for fsl-image-qt5-validation-imx

2,159件の閲覧回数
rthomas
Contributor III

Hello, I recently built the fsl-image-qt5-validation-imx image for the IMX8M Quad and meta-qt5 layer is included in that. I want to be able to have qmake in order to compile a qt program on the Yocto build. My question is, how do I get qmake to be there?

0 件の賞賛
返信
2 返答(返信)

2,142件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rthomas,

 

"qmake " is in the folder usr/bin and I can use qmake.

 

Problably you build is wrong because you have the meta-qt, i just can recommend to build you yocto project again.

 

Regards

 

0 件の賞賛
返信

1,627件の閲覧回数
shao-gaoyan
Contributor II

hello  Bio_TICFSL

bitbake -c populate_sdk imx-image-full

I did not find qmake in the SDK after executing the command, is this normal?

Looking forward to your reply

0 件の賞賛
返信