No Picture with DSI to LVDS bridge SN65DSI83

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Picture with DSI to LVDS bridge SN65DSI83

5,693 Views
thom
Contributor II

Hay Guys, 

i have the following problem.

I port the driver for the SN65DSI83 to the current Linux Kernel (4.14.98_2.0.0 from NXP). 

The Driver and dts are fine compilted and working (see log). But i dont get a picture on my Display. So i checked the Registers of the SN65DSI83 and all looks fine... 

Did anyone have a idea to fix this problem? 

Source of the Driver: 

https://github.com/varigit/linux-imx/tree/imx_4.14.78_1.0.0_ga_var01/drivers/gpu/drm/bridge/sn65dsi8...

Labels (1)
0 Kudos
Reply
9 Replies

4,304 Views
thom
Contributor II

Hay Guys, 

thx for the Help. I looks like an Issue in 4.14.98 Kernel. 

I compiled the 4.14.78 Kernel and its Working after so Hours of playing. 

Can anyone tell me what is the difference betwen 4.14.78 / 4.14.98 Kernel within DSI Configuration? 

I see with the Scope, the Data on the DSI Lanes are completly different. 

Now i use a 2 Lane Configuration with 422 MHz Clock.

0 Kudos
Reply

4,304 Views
rda_emcraft
Contributor I

Hello Thomas,

Can you, please, share your working DTS and point to exact SN65DSI83 driver version that works?

Dmitry

0 Kudos
Reply

4,304 Views
thorben
Contributor II

Hi Thomas,

have you been able to get 4.14.98 kernel running with SN65DSI83?

Thorben

0 Kudos
Reply

4,304 Views
thom
Contributor II

Hay guys, 

thx for the Informations. So i attach the .dts file. 

I use the imx8mmevk for testing currently. 

with kind of probe is missing there? 

I set the DSI Lanes to the rigth count (4) and the frequency is set to 213.3MHz. I see with the scope some data and the stable Clock. So i think the DSI Init would be fine there. 

0 Kudos
Reply

4,304 Views
felixradensky
Contributor IV

Hi Tomas,

There's no SN65DSI83 bridge on NXP EVK. Do you have it on some add-on card ?

Felix.

0 Kudos
Reply

4,304 Views
igorpadykov
NXP Employee
NXP Employee

in general also one can try to adjust custom specific lcd sctructures

struct cmd_set_entry manufacturer_cmd_set[], struct display_timing rad_default_timing

in linux/drivers/gpu/drm/panel/panel-raydium-rm67191.c

panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor

0 Kudos
Reply

4,304 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

one can check "display-timings" in fsl-imx8mq-evk-dcss-rm67191.dtsi file

linux-imx/fsl-imx8mq-evk-dcss-rm67191.dtsi at imx_4.14.78_1.0.0_ga_var01 · varigit/linux-imx · GitHu... 

DART-MX8M Display - Variscite Wiki 

Best regards
igor

0 Kudos
Reply

4,304 Views
felixradensky
Contributor IV

Hi Thomas,

Please check the number of DSI lanes in LVDS bridge DTS node. We have intentionally set it to 1 to workaround limitations of MIPI-DSI bridge driver in kernel 4.14.78. These limitations are supposed to be fixed in kernel 4.14.98, so you try using the real number of DSI lines supported by you panel.

If you're using Variscite DART-MX8M-MINI module you can ask for assistance on our Customer Portal 

Felix.

0 Kudos
Reply

4,304 Views
Niebel-TQ
Contributor IV

Hi,

depending on your exact setup:

driver stack maybe missing deferred probing

you maybe need to tweak pixel clock to make dsi driver happy

have you tried with lcdif and dcss?

Only few of the things I remember when playing around with DSI-To-X bridges from TI and NXP 4.14.78_1.0.0

0 Kudos
Reply