No PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No PWM

1,085 Views
tlamarc
Contributor I

I am trying to get a pwm signal on gpio 1 1 for an i.MX7s processor.  Here is my device tree configuration but I see nothing on the pin.  Any help would be greatly appreciated.

/ {

   pwm-leds {

   compatible = "pwm-leds";

      pwm_led1 {

         label = "pwm_led1";

         pwms = <&pwm1 0 100000 50000>;

         max-brightness = <255>;

      };

   };

};

 

&pwm1 {

   pinctrl-names = "default";

   pinctrl-0 = <&pinctrl_pwm_led1>;

   status = "okay";

};

 

&iomuxc {

   pinctrl_pwm_led1: pwm_led1 {

   fsl,pins = <

      MX7D_PAD_LPSR_GPIO1_IO01__PWM1_OUT 0x14

   >;

   };

};

0 Kudos
Reply
3 Replies

1,029 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Please change the driver according to this document.

Also, this solution provided by a colleague may help debug this issue.

Regards

0 Kudos
Reply

992 Views
tlamarc
Contributor I

I updated the line from:   compatible = "pwm-leds";

to:   compatible = "fsl,imx7d-pwm";

but I still have no pwm signal on the pin,

0 Kudos
Reply

951 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

You can base on 7d-sdb device tree,

pwm1: pwm@30660000 {
				compatible = "fsl,imx7d-pwm", "fsl,imx27-pwm";
				reg = <0x30660000 0x10000>;
				interrupts = <GIC_SPI 81 IRQ_TYPE_LEVEL_HIGH>;
				clocks = <&clks IMX7D_PWM1_ROOT_CLK>,
					 <&clks IMX7D_PWM1_ROOT_CLK>;
				clock-names = "ipg", "per";
				#pwm-cells = <3>;
				status = "disabled";
			};

...

&pwm1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_pwm1>;
	status = "okay";
};

...

- backlight: backlight {
- 		compatible = "pwm-backlight";
- 		pwms = <&pwm1 0 5000000 0>;
- 		brightness-levels = <0 4 8 16 32 64 128 255>;
- 		default-brightness-level = <6>;
- 		status = "okay";
- 	};

I reproduced in 8mp-evk with the device tree,

pwm1: pwm@30660000 {
				compatible = "fsl,imx8mp-pwm", "fsl,imx27-pwm";
				reg = <0x30660000 0x10000>;
				interrupts = <GIC_SPI 81 IRQ_TYPE_LEVEL_HIGH>;
				clocks = <&clk IMX8MP_CLK_PWM1_ROOT>,
					 <&clk IMX8MP_CLK_PWM1_ROOT>;
				clock-names = "ipg", "per";
				#pwm-cells = <3>;
				status = "disabled";
			};

...

&pwm1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_pwm1>;
	status = "okay";
};

And these steps from the post I mentioned,

root@imx8mpevk:~# cat /sys/class/pwm/pwmchip0/npwm
1
root@imx8mpevk:~# echo 0 > /sys/class/pwm/pwmchip0/export
root@imx8mpevk:~# ls /sys/class/pwm/pwmchip0/pwm0/
capture  duty_cycle  enable  period  polarity  power  uevent
root@imx8mpevk:~# echo 10000 > /sys/class/pwm/pwmchip0/pwm0/period
root@imx8mpevk:~# echo 2000 > /sys/class/pwm/pwmchip0/pwm0/duty_cycle
root@imx8mpevk:~# echo 1 > /sys/class/pwm/pwmchip0/pwm0/enable

JosephAtNXP_0-1714149539173.png

Regards,

0 Kudos
Reply