I'm trying to update the OS on a custom variscite imx6 board, installing android oreo, but I don't get LVDS output, only HDMI.
the board has a 30 pin lvds output and the display is LM230WF3-SLQ5. I don't need both video outputs at the same time, I just need lvds.
I have 2 VAR-SOM-MX6, one configured to output lvds with debian (but I don't know what configuration it has to achieve it, I don't have the source code), and the second in which I'm trying to get lvds output.
Since the one that works is on debian, my first attempt was to install debian (I used the Variscite recovery sd card) and try to get the correct configuration, and then apply it to android. For this I am connected by the serial port.
Comparing the configuration, I notice that both have the same configuration variable in u-boot, but in the boot logs I already begin to notice differences referent with split mode.
Where should I make the change to achieve the lvds output?
I share the output logs
I understand your point, but we can not support that because we do not use Debian.
Apologies for inconvenient.
Best regards.