No HDMI signal from Nitrogen6x board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No HDMI signal from Nitrogen6x board

3,992件の閲覧回数
PeterBergin
Contributor III

Hi,

I have built a image for my Nitrogen6x board with Yocto and the daisy branch with linux-boundary 3.10 kernel. When booting my board I can not get any signal out of HDMI. I hope someone can help me with some ideas!

root@nitrogen6x:~# uname -a

Linux nitrogen6x 3.10.17-1.0.0_ga+yocto+g731f96d #1 SMP Wed May 21 12:09:44 CEST 2014 armv7l GNU/Linux

root@nitrogen6x:~# cat /proc/cmdline

enable_wait_mode=off video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=28M console=ttymxc1,115200 vmalloc=400M consoleblank=0 rootwait root=/dev/mmcblk0p2

Some printouts from the serial console:

mxc_sdc_fb fb.27: 1920x1080 h_sync,r,l: 44,88,148  v_sync,l,u: 5,4,36 pixclock=148500000 Hz

mxc_sdc_fb fb.27: timeout when waiting for flip irq

mxc_sdc_fb fb.27: timeout when waiting for flip irq

mxc_sdc_fb fb.27: 1920x1080 h_sync,r,l: 44,88,148  v_sync,l,u: 5,4,36 pixclock=148500000 Hz

mxc_sdc_fb fb.27: timeout when waiting for flip irq

mxc_sdc_fb fb.27: timeout when waiting for flip irq

Loading kernel module for a network device with CAP_SYS_MODULE (deprecated).  Use CAP_NET_ADMIN and alias netdev- instead.

mxc_sdc_fb fb.27: timeout when waiting for flip irq

mxc_sdc_fb fb.27: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb fb.27: timeout when waiting for flip irq

mxc_sdc_fb fb.27: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb fb.27: timeout when waiting for flip irq

mxc_sdc_fb fb.27: MXCFB_WAIT_FOR_VSYNC: timeout 0

I have tried with three different displays/TVs with similar result. I have tried HDMI-HDMI and HDMI-DVI cable with similar behaviour.

One observation is that u-boot can display content on the screen. When entering u-boot console the version of u-boot is displayed. u-boot can also read EDID information from the screen.

U-Boot 2014.04 (May 19 2014 - 15:20:05)

CPU:   Freescale i.MX6Q rev1.0 at 792 MHz

Reset cause: POR

Board: Nitrogen6X

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB

auto-detected panel HDMI

Display: HDMI (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   using phy at 6

FEC [PRIME], usb_ether

Hit any key to stop autoboot:  0

U-Boot > i2c edid 0x50

EDID version: 1.3

Product ID code: 069f

Manufacturer: SAM

Serial number: 43423234

Manufactured in week: 44 year: 2010

Video input definition: digital signal, voltage level 0

Monitor is non-RGB

Maximum visible display size: 52 cm x 29 cm

Power management features: active off, no suspend, no standby

Estabilished timings:

        720x400         70 Hz (VGA 640x400, IBM)

        640x480         60 Hz (VGA)

        640x480         67 Hz (Mac II, Apple)

        640x480         72 Hz (VESA)

        640x480         75 Hz (VESA)

        800x600         56 Hz (VESA)

        800x600         60 Hz (VESA)

        800x600         72 Hz (VESA)

        800x600         75 Hz (VESA)

        832x624         75 Hz (Mac II)

        1024x768        60 Hz (VESA)

        1024x768        70 Hz (VESA)

        1024x768        75 Hz (VESA)

        1280x1024       75 (VESA)

        1152x870        75 (Mac II)

Standard timings:

        1280x800        60 Hz

        1280x960        60 Hz

        1280x1024       60 Hz

        1440x900        60 Hz

        1600x1200       60 Hz

        1680x1050       60 Hz

        1152x864        75 Hz

        1440x900        75 Hz

        1920x1080       60 Hz (detailed)

Monitor range limits, horizontal sync: 30-81 kHz, vertical refresh: 56-75 Hz, max pixel clock: 170 MHz

Monitor name: SMB2440L

Monitor serial number: H9XZB00475

U-Boot >

I have also tested with a prebuilt image from Boundary http://boundarydevices.com/yocto-kernel-3-10-17-beta/

With this image I get same behaviour. No signal output on HDMI.

The console:

starting statd: done

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb fb.25: 1280x720 h_sync,r,l: 40,110,220  v_sync,l,u: 5,5,20 pixclock=74250000 Hz

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

mxc_sdc_fb fb.25: timeout when waiting for flip irq

vgaarb: this pci device is not a vga device

Starting advanced power management daemon: No APM support in kernel

(failed.)

NFS daemon support not enabled in kernel

Starting smarthome

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb fb.25: 1280x720 h_sync,r,l: 40,110,220  v_sync,l,u: 5,5,20 pixclock=74250000 Hz

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb fb.25: 1280x720 h_sync,r,l: 40,110,220  v_sync,l,u: 5,5,20 pixclock=74250000 Hz

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

vgaarb: this pci device is not a vga device

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb fb.25: 1920x1080 h_sync,r,l: 44,528,148  v_sync,l,u: 5,4,36 pixclock=148500000 Hz

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

libphy: 2188000.ethernet:06 - Link is Up - 100/Half

Starting syslogd/klogd: done

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb fb.25: 1920x1080 h_sync,r,l: 44,528,148  v_sync,l,u: 5,4,36 pixclock=148500000 Hz

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb fb.25: 1920x1080 h_sync,r,l: 44,528,148  v_sync,l,u: 5,4,36 pixclock=148500000 Hz

   ...done.

Starting Telephony daemon

Starting Linux NFC daemon

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

Starting OProfileUI server

Running local boot scripts (/etc/rc.local).

Stopping Bootlog daemon: bootlogd.

Poky (Yocto Project Reference Distro) 1.5+snapshot-20140302 nitrogen6x /dev/ttymxc1

nitrogen6x login: Unable to load library icui18n "Cannot load library icui18n: (icui18n: cannot open shared object file: No such file or directory)"

smarthome: cannot connect to X server

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb fb.25: 1920x1080 h_sync,r,l: 44,528,148  v_sync,l,u: 5,4,36 pixclock=148500000 Hz

Thanks,

/Peter

6 返答(返信)

1,284件の閲覧回数
EricNelson
Senior Contributor II

Following up for those not on the meta-freescale list. This appears to be a problem only with older silicon (TO1.0).

     https://lists.yoctoproject.org/pipermail/meta-freescale/2014-May/008672.html

0 件の賞賛
返信

1,284件の閲覧回数
mohammedazlum
Contributor IV

Hello,

I have faced same smarthome: cannot connect to X server issue. This problem observed (my case) when I connected 120 Ohm impedance common mode choke between HDMI connector and iMX6 processor. When I replaced the choke with 90 Ohm impedance the problem got solved.

Regards,

Azlum

0 件の賞賛
返信

1,284件の閲覧回数
controlhorus
Contributor III

Hello

Similar thing here. We started to try Daisy on a SabreLite board two days ago. We tested with inux-imx kernel 3.10.17. U-boot see the HDMI monitor. Linux does not see it. Xserver does not start. And Qt application does not find icui18n library.

Best regards,

Jose

0 件の賞賛
返信

1,284件の閲覧回数
EricNelson
Senior Contributor II

Hi Diego,

I just noticed some things in your message:

  • You mention using 'linux-imx'. Can you try using 'linux-boundary'? That's what we've tested, since there are lots of omissions in the DT in 'linux-imx'.
  • You mention some issues with Qt and libicu. These are probably best answered through the meta-freescale mailing list or at least as a separate topic for clarity. They likely have nothing to do with the HDMI issue which is the subject of this post.
0 件の賞賛
返信

1,284件の閲覧回数
EricNelson
Senior Contributor II

Hi Diego,

Note that I'm currently tracking this on the meta-freescale mailing list.

https://lists.yoctoproject.org/pipermail/meta-freescale/2014-May/008553.html

I have a suspicion that the issue stems from a missing "mxc_hdmi.only_cea=1" in the kernel command-line.

0 件の賞賛
返信

1,284件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello

Boundary Devices

Can you please comment on customer issue?

0 件の賞賛
返信