No HDMI output on SCM-i.MX6DQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No HDMI output on SCM-i.MX6DQ

1,371 Views
stephanhoffmann
Contributor III

Hello,

I've got a SCM-i.MX6DUal/6Quad Quick Start Board and followed the Quick Start Guide. Unfortunatelly, I do not get any output on two different Monitors connected to the HDMI port. Both monitors work with any other HDMI source I tried previously.

On the serial console I get the following messages:

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

The firmware is as delivered (extract from boot messages):

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Dec 03 2016 - 13:47:20 -0600)CPU: Freescale i.MX6Q rev1.5 at 792MHz
CPU: Commercial temperature grade (0C to 95C) at 29C
Reset cause: POR
Board: MX6DQSCM-QWKS-REV3
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
reading imx6dqscm-1gb-qwks-rev3-fix-ldo.dtb

Linux version 4.1.15-2.0.0+gb63f3f5 (jgutierrez@bluedemon) (gcc version 5.3.0 (GCC) ) #1 SMP PREEMPT Sat Dec 3 13:50:35 CST 2016

I already returned one unit because I thought the HDMI might be broken, but the new one shows the same behaviour.

Kind regards

Stephan

Labels (1)
2 Replies

1,120 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Stephan,

Try to change the uboot version, the previous u-boot is sending a bad parameter for loading the kernal. so when a HDMI is needed it shows the error. After changing the U-boot the error is not showing as well as the HDMI is working properly

1,120 Views
260738521
Contributor I

hi,

  I use the 2019 Dec.newest uboot and kernel. but I've got this problem too." imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready"

0 Kudos