Dear all,
I have some problems to get the ADB Interface on the host using target FSL iMX51 BABBAGE 3.0 and BSP R10.3.
My PC drivers are fine. My GUI settings are fine (Settings > Applications > Development > USB debugging). The ADB Interface is just missing in the USB Descriptors (verified with "lsusb" on Linux, and "usbview" on Windows).
In kernel .config, the Android gadget drivers are enabled:
CONFIG_USB_ANDROID=y
CONFIG_USB_ANDROID_ADB=y
CONFIG_USB_ANDROID_MASS_STORAGE=y
CONFIG_USB_ANDROID_RNDIS=y
CONFIG_USB_ANDROID_RNDIS_WCEIS=y
In kernel_imx/arch/arm/mach-mx5/mx51_babbage.c, the Android gadget functions are configured. Here, USB ProductID 0x0c01 is set as default, which corresponds with the "usb_mass_storage" function.
Normally, USB ProductID 0x0c02 appears immediately, which has both "USB Mass Storage" and "ADB Interface".
During kernel boot, below messages are printed.
(Extra prints were added to kernel_imx/drivers/usb/gadget/)
CPU is i.MX51 Revision 3.0
mx51_babbage.c mxc_board_init(): ready to mxc_register_device(android_usb_device) with following android_usb_platform_data: vendorID 5538, productID 3073, productname MX51 BBG Android
...
Android usb driver initialize
android_usb gadget: composite.c adding config #1 'android'/80900164
android_usb gadget: composite.c cfg 1/80900164 speeds:
android.c product_matches_functions(): product 3073 matches
android.c get_product_id() returning 3073
android_usb gadget: android_usb ready
fsl-usb2-udc: bind to driver android_usb
android_usb gadget: composite.c suspend
android gadget: register function adb
android gadget: register function usb_mass_storage
android gadget: register function rndis
rndis_function_bind_config MAC: 00:00:00:00:00:00
android_usb gadget: using random self ethernet address
android_usb gadget: using random host ethernet address
usb0: MAC 3a:e4:91:cd:ff:47
usb0: HOST MAC a2:55:77:31:d3:e8
android_usb gadget: composite.c adding 'rndis'/990c8780 to config 'android'/80900164
android_usb gadget: usb_mass_storage, version: 2009/09/11
android_usb gadget: Number of LUNs=3
lun0: LUN: removable file: (no medium)
lun1: LUN: removable file: (no medium)
lun2: LUN: removable file: (no medium)
android_usb gadget: composite.c adding 'usb_mass_storage'/99293240 to config 'android'/80900164
android_usb gadget: composite.c adding 'adb'/990c89c0 to config 'android'/80900164
android_usb gadget: f_adb.c adb_function_bind dev: 990c89c0
android_usb gadget: f_adb.c create_bulk_endpoints dev: 990c89c0
android_usb gadget: f_adb.c usb_ep_autoconfig for ep_in got ep4in
android_usb gadget: f_adb.c usb_ep_autoconfig for adb ep_out got ep3out
android_usb gadget: f_adb.c dual speed adb: IN/ep4in, OUT/ep3out
android_usb gadget: composite.c resume
...
android_usb gadget: composite.c HNP inactive
android_usb gadget: high speed config #1: android
On the iMX51 target, process /sbin/adbd is running.
When explicitly and dynamically enabling adb on the shell:
echo 1 > /sys/devices/virtual/usb_composite/adb/enable
USB ProductID 0x0c01 (3073) is replaced by 0x0c02 (3074). On the PC, ADB Interface appears, usbview shows:
bInterfaceClass: 0xFF
bInterfaceSubClass: 0x42
bInterfaceProtocol: 0x01
These values are ADB_CLASS, ADB_SUBCLASS and ADB_PROTOCOL from system/core/adb/adb.h
Looks good, but...ADB Interface is offline ("adb devices"):
List of devices attached
0123456789ABCDEF offline
When you reboot the iMX51, it has again USB ProductID 0x0c01 (3073) and no ADB Interface.
When enabling adb on the shell, the kernel prints:
(Extra prints were added to kernel_imx/drivers/usb/gadget/)
composite.c usb_function_set_enabled(): set function adb to 1
android.c product_has_function(): product 3073 has NO function rndis
android.c product_has_function(): product 3073 has function usb_mass_storage
android.c product_has_function(): product 3073 has NO function adb
android.c product_matches_functions(): product 3073 does NOT match
android.c product_has_function(): product 3074 has NO function rndis
android.c product_has_function(): product 3074 has function usb_mass_storage
android.c product_has_function(): product 3074 has function adb
android.c product_matches_functions(): product 3074 matches
android.c get_product_id() returning 3074
android_usb gadget: composite.c reset config
android_usb gadget: f_adb.c adb_function_disable
android_usb gadget: f_adb.c adb disabled
android_usb gadget: composite.c suspend
Any clue why the ADB Interface is not enabled automatically/dynamically?
Note that the prebuilt image by Freescale (from image_imx-android-r10.3_51bbg) is OK:
USB ProductID 0x0c02 (3074) appears immediately (no switch from 0x0c01) with both USB Mass Storage and ADB Interface:
ADB Interface is ready ("adb devices"):
List of devices attached
0123456789ABCDEF device
Thanks a lot,
Tom.
5.9 How to setup PC (Windows) to support ADB/RNDIS
Before this release, we used HTC's vendor id and product id for all the android gadget functions. It's bad case, so we changed the default android USB gadget functions's VendorID to freescale's 0x15a2, and ProductID to fake ones(after acquiring the offical product id, we will replace them). Due to this change, we must update the PC's USB driver and ADB configuration to enable the android gadget functions:
For Windows PC:
For Linux PC:
| # ANDROID 3RD PARTY USB VENDOR ID LIST -- DO NOT EDIT. # USE 'android update adb' TO GENERATE. # 1 USB VENDOR ID PER LINE. 0x15a2 |
| SUBSYSTEM=="usb", SYSFS{idVendor}=="15a2", MODE="0666" |
the weird thing is that you can see the device. But it´s offline.
I have never faced this!
if you figure out the root cause, please share.
Thanks both for your reply.
I double-checked ~/.android/adb_usb.ini and %USERPROFILE%\.android\adb_usb.ini but the file contained the Freescale USB Vendor ID already...
For now, I am using ADB over Ethernet as a workaround.
Will look into the differences later.
Tom,
Sorry for the poll this much later.....
...but did you ever get adb working over USB for the Mx51?
I think I'm following in your footsteps. :smileysad:
thanks for any input,
Mike
"Note that the prebuilt image by Freescale (from image_imx-android-r10.3_51bbg) is OK:"
It seems to me that there's your answer. The prebuilt image's exact source code will be provided to you (as per the GPLv2).
If you compile that source code, it should work (otherwise it's a compilation problem).
So then you can compare (hint: diff -Nabur) that version to yours and track down the change that caused the problem...
What did you change on your code?
Would you be missing to change ~/.android/adb_usb.ini for your case?