Nitrogen8m SOM - Boundary devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nitrogen8m SOM - Boundary devices

1,024 Views
srinu_inaganti
Contributor III

Hi,

1. I want use UART1 for RS232 communication. for RTS and CTS lines i want use UART4_Tx and UART_Rx. Is that the right way to do ? How to change the device tree for this configuration.

2. And also anyone help me to write a device tree changes procedure to connect I2C expander to I2C3 bus. 

3. How to write a device tree for registering the pins for GPIO.

Thanks in Advance,

Srinu Inaganti

1 Reply

943 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinu

from Reference Manual UART1 RTS and CTS are available on UART3, not UART4

pastedImage_2.jpg

both UART3,4 are used on board:

linux-imx6/imx8mq-nitrogen8m_som.dts at boundary-imx_4.14.x_2.0.0_ga · boundarydevices/linux-imx6 · ... 

for device tree customization one can look at

https://boundarydevices.com/mx6-device-tree-customization/ 

This board was produced by boundary devices and issue may be posted on its

forum: https://boundarydevices.com/wiki/nitrogen8m-som/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------