Nitrogen i.MX8MM Ethernet Issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nitrogen i.MX8MM Ethernet Issues

1,513件の閲覧回数
nbutts
Contributor I

I'm having a lot of issues with Ethernet working reliably on a Nitrogen i.MX8MM device. Sometimes I get a

MDIO write timeout

in the system log, otherwise the interface just goes down. I tried resetting the phy, but once Ethernet drops I have to remove power for several seconds and then reapply power. It will then work for a minute or so.

root@bionic-dev64:~# mii-tool -r eth0
restarting autonegotiation...
root@bionic-dev64:~# ifcon[   93.852651] fec 30be0000.ethernet eth0: MDIO write timeout
fig
eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
        inet 192.168.110.121  netmask 255.255.255.0  broadcast 192.168.110.255
        inet6 fe80::219:b8ff:fe06:af3b  prefixlen 64  scopeid 0x20<link>
        ether 00:19:b8:06:af:3b  txqueuelen 1000  (Ethernet)
        RX packets 152  bytes 17908 (17.9 KB)
        RX errors 33  dropped 0  overruns 0  frame 41
        TX packets 127  bytes 16411 (16.4 KB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
I have Rx errors 
0 件の賞賛
返信
2 返答(返信)

1,332件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nick Butts,


The Nitrogen i.MX8MM is manufactured and supported by Boundary Devices. gary_bisson, would you have any suggestion of what may be the issue here?

Regards,

0 件の賞賛
返信

1,332件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

I'm no longer with Boundary Devices.

Please contact support@boundarydevices.com directly.

Regards,

Gary