Hi,
I am using nitrogen 8M (boundary device board), when trying to configuration partition through U-Boot. I have gave comand like "mmc partconf 0 1 0 0" accidentaly, after that i am not able to see my U-Boot serial console.
So recover it, I have also tried System recovery option to flash u-boot through Serial Download. I am able to successfully the flash it, still U-Boot is not working.
I have followed following steps
1. As suggested in the below, I have built Boundary device uboot for imx8 in the Building for i.MX8 section
https://boundarydevices.com/u-boot-v2018-07/
2. Then pulled the latest imx_usb_loader from: https://github.com/boundarydevices/imx_usb_loader
And I kept both imx_usb_loader and u-boot in the same directory. Then tried to run imx_usb_loader as follows:
sudo ./imx_usb
3. Repeated the step again. That is-> sudo ./imx_usb
Please check attachment, I have given the steps executed in the machine . And please help me to unbrick the devices.
Regards,
Ashok S
Hi,
Please use uuu to unbrick the device as explained here:
https://boundarydevices.com/recovering-i-mx-platforms-using-uuu/
Regards,
Gary
Hello Ashok S,
This board is manufactured and supported by Boundary Devices. While hopefully a community user may have experience with this board and provide some help, I would recommend that you contact Boundary Devices for help.
My apologies for the inconvenience.
Regards,