Nitrogen 6X - can not get cameras operational.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nitrogen 6X - can not get cameras operational.

Jump to solution
1,502 Views
cristianpandele
Contributor II

Hello,

I received my Bounday Devices Nitrogen 6X board yesterday, together with the two OV5640 cameras (the parallel and MIPI versions).

I have since tried the bundled Yocto version, the Yocto Fido release and now I am on the 2015 release of Ubuntu Trusty, and under none of the versions have I managed to run the simplest gstreamer command taking input video from the cameras. The only improvement under Ubuntu is that HDMI finally works, but that is a secondary issue,

So, back to the cameras. With only the MIPI camera plugged in, this is what I run right after boot:

modprobe ov5640_camera_mipi

modprobe mxc_v4l2_capture

(the drivers do show up properly in lsmod afterwards)

sudo gst-launch imxv4l2src ! imxv4l2sink 

MFW_GST_V4LSRC_PLUGIN 4.0.2 build on Jun  1 2015 05:36:19.mxc_v4l_open: Mxc C

amera no sensor ipu0/csi0

mxc_v4l_open: Mxc Camera no sensor ipu0/csi1

mxc_v4l_open: Mxc Camera no sensor ipu0/csi0

MFW_GST_V4LSINK_PLUGIN 4.0.2 build on Jun  1 2015 05:35:56mxc_v4l_open: Mxc C

amera no sensor ipu0/csi0

.

Setting pipeline to PAUSED ...

ERROR: Pipeline doesn't want to pause.

Setting pipeline to NULL ...

Total rendered:0

Freeing pipeline ...

[--->FINALIZE v4l_sink

However, the MIPI camera seems to be detected at boot:

dmesg | grep ov56          
ov5640_read_reg:write reg error:reg=300a                                  
camera ov5640 is not found                                                
ov5640_mipi 1-003e: found pwm2, period=45                                 
mxc_v4l2_master_attach: ipu1:/csi0 mipi attached ov5640_mipi:mxc_v4l2_cap1
camera ov5640_mipi is found                                               
update_device_addr: ov5642 ret=-5                                         
ov5642_read_reg:write reg error:reg=300a                                  

camera ov5642 is not found 

Could anyone advise me on what next to take? I have tried following similar threads in the past day and a half, but none of the suggestions applied to my case. Please let me know what extra info I can post.

Thank you very much in advance!

Labels (3)
0 Kudos
1 Solution
902 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian

according to this post:

https://boundarydevices.com/compiling-latest-u-boot-for-i-mx6-2015-edition/

need the new 2015-07 boundary u-boot to work with the new 3.14.28 kernel.

https://www.mail-archive.com/meta-freescale@yoctoproject.org/msg16366.html//www.mail-archive.com/meta-freescale@yoctoproject.org/msg16366.html

https://github.com/boundarydevices/linux-imx6/commit/2ffd4a4

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
903 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian

according to this post:

https://boundarydevices.com/compiling-latest-u-boot-for-i-mx6-2015-edition/

need the new 2015-07 boundary u-boot to work with the new 3.14.28 kernel.

https://www.mail-archive.com/meta-freescale@yoctoproject.org/msg16366.html//www.mail-archive.com/meta-freescale@yoctoproject.org/msg16366.html

https://github.com/boundarydevices/linux-imx6/commit/2ffd4a4

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
902 Views
cristianpandele
Contributor II

Hi Igor,

Thank you for your message! I updated the u-boot script, and that seemed to do the trick!

However, I noticed that if I specify a different /dev/videoX to imxv4l2src, I get the same error messages as before. Could it be that imxv4l2 did not point to the correct video device as a source in the first instance? (given that there was only one camera present, it should have been the only valid source).

How can I programmatically determine which video device the cameras are attached to? If I type:

dmesg | grep video, I get:

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

mxc_v4l2_output v4l2_out.35: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.35: V4L2 device registered as video17

So nothing about the cameras being registered as specific devices.

Kindest regards,

Cristian Pandele

0 Kudos
902 Views
kende
Contributor I

Hullo,

You could parse the output of "v4l2-ctl --list-devices" or use its sources to write your own detector.

--

Kende

902 Views
cristianpandele
Contributor II

Hi Kende,

Great tip, thanks! I didn't have v4l-utils installed, a lot of great stuff that can be used from there!

Kindest regards,

Cristian Pandele

0 Kudos
902 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian

boundary devices developers are working on 

meta-fsl-arm mailing list, so for more details one can post on

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 Kudos