Next planned Stable imx6 Kernel Release?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Next planned Stable imx6 Kernel Release?

1,386 Views
dilshad_alam
Senior Contributor II

After imx_3.14.28_1.0.0_ga which one is next planned Stable Kernel Release?

Labels (1)
5 Replies

1,203 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Next release includes 3.14.38 kernel; it is already mentioned on i.MX6UL documents:

http://www.freescale.com/files/32bit/doc/app_note/AN5170.pdf


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,203 Views
hurroz
Contributor I

Hi, when will 3.14.38 become available?

0 Kudos

1,203 Views
dilshad_alam
Senior Contributor II

Thanks for your reply.

Any plans to go for Kernel 4.0. Most of the vendors are taking baseline as vanilla kernel 4.0.

0 Kudos

1,203 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

There are no plans of a software release using kernel 4.0 at least for this year (2015). You could be aware of additional releases on i.MX webpage at www.freescale.com/imx

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,203 Views
dilshad_alam
Senior Contributor II

Thanks for your reply. I don't see any future kernel releases section in that link.

0 Kudos