Dear sirs
I have a problem in downloading the programs to a new imx6ul-board using mfgtools, please see the attached file.
How can i deal with the problem, thanks a lot!
BR
Hi, qizhi wang
Please refer below link which may help you.
https://community.nxp.com/thread/454298
Regards,
Shivani
hi,Shivani
Thanks for your reply.
yes, I am trying to flash images in nandflash. I did it according the third-party's Board programs, please see the attached files, could you show me where the problem is? Thank you.
BEST REGARDS
WANG QIZHI
Hi, wangqz2010@126.com
I can not see any attached files here. Have you attached some other files or the one you have attached in the main question?
Regards,
Shivani
Hi, Shivani
Could you tell what's the problem about the following messages? Thanks.
REGARDS
WQZ
U-Boot 2015.04-g5d63276bfe-dirty (Jan 10 2017 - 15:40:43)
CPU: Freescale i.MX6UL rev1.2 at 396 MHz
CPU: Temperature 47 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 256 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
MMC: no card present
MMC init failed
Using default environment
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
MMC: no card present
Net: FEC1
Error: FEC1 address not set.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz $ $ $;
Hit any key to stop autoboot: 0
Kernel image @ 0x80800000
Loading init Ramdisk from Legacy Image at 83800000 ...
Image Name: fsl-image-mfgtool-initramfs-imx_
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7485694 Bytes = 7.1 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300c60a
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.14.38+ (root@develop) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #4 SMP PREEMPT Mon Jan 9 09:53:31 CST 2017
CPU: ARMv7 Processor revision 5 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
cma: CMA: reserved 64 MiB at 8c000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @8bdbf000 s8320 r8192 d16256 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc cma=64m g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 176672K/262144K available (6712K kernel code, 347K rwdata, 2216K rodata, 360K init, 418K bss, 85472K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0x90800000 - 0xff000000 (1768 MB)
lowmem : 0x80000000 - 0x90000000 ( 256 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x808c02e8 (8929 kB)
.init : 0x808c1000 - 0x8091b080 ( 361 kB)
.data : 0x8091c000 - 0x80972fa0 ( 348 kB)
.bss : 0x80972fac - 0x809dba50 ( 419 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
clocksource_of_init: no matching clocksources found
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x8065f4f8 - 0x8065f568
Brought up 1 CPUs
SMP: Total of 1 processors activated (6.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap registered
vdd3p0: 2625 <--> 3400 mV at 3000 mV
cpu: 725 <--> 1450 mV at 1150 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e4000.iomuxc-gpr: regmap registered
syscon 21ac000.romcp: regmap registered
syscon 21bc000.ocotp-ctrl: regmap registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/csi1grp
imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/i2c2grp
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
20dc000.gpc supply pu not found, using dummy regulator
bio: create slab <bio-0> at 0
mxs-dma 1804000.dma-apbh: initialized
can-3v3: 3300 mV
VSD_3V3: 3300 mV
usb_otg1_vbus: 5000 mV
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
cfg80211: Calling CRDA to update world regulatory domain
NET: Registered protocol family 2
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7304K (83801000 - 83f23000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 487
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight.8 supply power not found, using dummy regulator
MIPI DSI driver module loaded
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 100x30
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.1
imx-sdma 20ec000.sdma: initialized
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
console enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62, base_baud = 5000000) is a IMX
serial: Freescale lpuart driver
imx sema4 driver is registered.
Initialized drm 1.1.0 20060810
Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
nand: Could not find valid ONFI parameter page; aborting
nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xd3
nand: Micron NAND 1GiB 3,3V 8-bit
nand: 1024MiB, SLC, page size: 4096, OOB size: 128
Scanning device for bad blocks
gpmi-nand 1806000.gpmi-nand: DMA timeout, last DMA :1
gpmi-nand 1806000.gpmi-nand: Show GPMI registers :
gpmi-nand 1806000.gpmi-nand: offset 0x000 : 0x21800080
gpmi-nand 1806000.gpmi-nand: offset 0x010 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x020 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x030 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x040 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x050 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x060 : 0x0104000c
gpmi-nand 1806000.gpmi-nand: offset 0x070 : 0x00010203
gpmi-nand 1806000.gpmi-nand: offset 0x080 : 0x05000000
gpmi-nand 1806000.gpmi-nand: offset 0x090 : 0x23023336
gpmi-nand 1806000.gpmi-nand: offset 0x0a0 : 0xffffffff
gpmi-nand 1806000.gpmi-nand: offset 0x0b0 : 0xff000005
gpmi-nand 1806000.gpmi-nand: offset 0x0c0 : 0x00000100
gpmi-nand 1806000.gpmi-nand: offset 0x0d0 : 0x05020000
gpmi-nand 1806000.gpmi-nand: Show BCH registers :
gpmi-nand 1806000.gpmi-nand: offset 0x000 : 0x00000100
gpmi-nand 1806000.gpmi-nand: offset 0x010 : 0x00000010
gpmi-nand 1806000.gpmi-nand: offset 0x020 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x030 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x040 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x050 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x060 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x070 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x080 : 0x070a2080
gpmi-nand 1806000.gpmi-nand: offset 0x090 : 0x10802080
gpmi-nand 1806000.gpmi-nand: offset 0x0a0 : 0x070a4080
gpmi-nand 1806000.gpmi-nand: offset 0x0b0 : 0x10da4080
gpmi-nand 1806000.gpmi-nand: offset 0x0c0 : 0x070a4080
gpmi-nand 1806000.gpmi-nand: offset 0x0d0 : 0x10da4080
gpmi-nand 1806000.gpmi-nand: offset 0x0e0 : 0x070a4080
gpmi-nand 1806000.gpmi-nand: offset 0x0f0 : 0x10da4080
gpmi-nand 1806000.gpmi-nand: offset 0x100 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x110 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x120 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x130 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x140 : 0x00000000
gpmi-nand 1806000.gpmi-nand: offset 0x150 : 0x20484342
gpmi-nand 1806000.gpmi-nand: offset 0x160 : 0x01000000
gpmi-nand 1806000.gpmi-nand: offset 0x170 : 0x00000000
gpmi-nand 1806000.gpmi-nand: BCH Geometry :
GF length : 13
ECC Strength : 8
Page Size in Bytes : 4224
Metadata Size in Bytes : 10
ECC Chunk Size in Bytes: 512
ECC Chunk Count : 8
Payload Size in Bytes : 4096
Auxiliary Size in Bytes: 20
Auxiliary Status Offset: 12
Block Mark Byte Offset : 3995
Block Mark Bit Offset : 0
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
.
.
.
.
.
.
.
.
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
8 ofpart partitions found on MTD device gpmi-nand
Creating 8 MTD partitions on "gpmi-nand":
0x000000000000-0x000000800000 : "boot"
0x000000800000-0x000000a00000 : "logo"
0x000000a00000-0x000000b00000 : "ENV"
0x000000b00000-0x000000e00000 : "DTB"
0x000000e00000-0x000001600000 : "kernel"
0x000001600000-0x000001700000 : "DTBbak"
0x000001700000-0x000001f00000 : "kernelbak"
0x000001f00000-0x000040000000 : "rootfs"
gpmi-nand 1806000.gpmi-nand: driver registered.
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 20b4000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
fec 20b4000.ethernet (unregistered net_device): Using random MAC address: 86:29:9b:2c:72:c8
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unregistered net_device): Using random MAC address: 8e:1d:09:65:ab:39
fec 2188000.ethernet eth1: registered PHC device 1
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
rtc-rx8010 0-0032: Unable to write register #23
i2c i2c-0: probing for rx8010 failed
rtc-rx8010: probe of 0-0032 failed with error -5
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
pxp-v4l2 pxp_v4l2.9: initialized
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
Registering SWP/SWPB emulation handler
usb_otg1_vbus: disabling
VSD_3V3: disabling
can-3v3: disabling
regulator-dummy: disabling
imx mcc test is registered.
Number of LUNs=8
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
Number of LUNs=1
LUN: removable file: (no medium)
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
clk: Not disabling unused clocks
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 360K (808c1000 - 8091b000)
Starting UTP
uuc 0.5
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
UTP: received command '$ cat /proc/mtd '
UTP: executing "cat /proc/mtd "
dev: size erasesize name
mtd0: 00800000 00040000 "boot"
mtd1: 00200000 00040000 "logo"
mtd2: 00100000 00040000 "ENV"
mtd3: 00300000 00040000 "DTB"
mtd4: 00800000 00040000 "kernel"
mtd5: 00100000 00040000 "DTBbak"
mtd6: 00800000 00040000 "kernelbak"
mtd7: 3e100000 00040000 "rootfs"
UTP: sending Success to kernel for command $ cat /proc/mtd .
utp_poll: pass returned.
UTP: received command '$ flash_eraseall /dev/mtd0'
UTP: executing "flash_eraseall /dev/mtd0"
flash_eraseall has been replaced by `flash_erase 0 0`; please use it
Erasing 256 Kibyte @ 0 -- 0 % cgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
omplete libmtd: error!: MEMERASE64 ioctlgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
failed for eraseblock 0 (mtd0)
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
error 5 (Input/output errgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
or)
flash_erase: error!: /dev/mtgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
d0: MTD Erase failure
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
error 5 (Input/output error)
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
Erasing 256 Kibyte @ 40000 -- 3gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
% complete libmtd: error!: MEMERgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
ASE64 ioctl failed for eraseblockgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
1 (mtd0)
error 5 (Inputgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
/output error)
flash_erase: errogpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
error 5 (Input/outpgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
ut error)
Erasing 256 Kibyte @ gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
80000 -- 6 % complete libmtd: ergpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
ror!: MEMERASE64 ioctl failed forgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
eraseblock 2 (mtd0)
errgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
or 5 (Input/output error)
flash_gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
erase: error!: /dev/mtd0: MTD Eragpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
se failure
error 5 (Input/output error)
Erasing 256 Kibyte @ c0000 -- 9 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 3 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 100000 -- 12 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 4 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 140000 -- 15 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 5 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 180000 -- 18 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 6 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 1c0000 -- 21 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 7 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 200000 -- 25 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 8 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 240000 -- 28 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 9 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 280000 -- 31 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 10 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 2c0000 -- 34 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 11 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 300000 -- 37 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 12 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 340000 -- 40 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 13 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 380000 -- 43 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 14 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 3c0000 -- 46 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 15 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 400000 -- 50 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 16 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 440000 -- 53 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 17 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 480000 -- 56 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 18 (mtd0)
error 5 (Input/output error)
flash_erase: errgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
or!: /dev/mtd0: MTD Erase failuregpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
error 5 (Input/outgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
put error)
Erasing 256 Kibyte @gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
4c0000 -- 59 % complete libmtd: gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
error!: MEMERASE64 ioctl failed fgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
or eraseblock 19 (mtd0)
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
error 5 (Input/output error)
flagpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
sh_erase: error!: /dev/mtd0: MTD gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
Erase failure
errorgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
5 (Input/output error)
Erasinggpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
256 Kibyte @ 500000 -- 62 % compgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
lete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 20 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 540000 -- 65 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 21 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 580000 -- 68 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 22 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 5c0000 -- 71 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 23 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 600000 -- 75 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 24 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 640000 -- 78 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 25 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 680000 -- 81 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 26 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtutp_poll: pass returned.
d0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 6c0000 -- 84 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 27 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 700000 -- 87 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 28 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 740000 -- 90 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 29 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 780000 -- 93 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 30 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 7c0000 -- 96 % complete libmtd: error!: MEMERASE64 ioctl failed for eraseblock 31 (mtd0)
error 5 (Input/output error)
flash_erase: error!: /dev/mtd0: MTD Erase failure
error 5 (Input/output error)
Erasing 256 Kibyte @ 7c0000 -- 100 % complete
UTP: sending Success to kernel for command $ flash_eraseall /dev/mtd0.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ ls $FILE'
UTP: executing "ls $FILE"
/tmp/file.utp
UTP: sending Success to kernel for command $ ls $FILE.
utp_poll: pass returned.
UTP: received command '$ kobs-ng init -x $FILE '
UTP: executing "kobs-ng init -x $FILE "
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
mtd: device 0 fails MEMERASE (0x0gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
- 0x40000)
mtd: Failed to erasegpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
block @0x0
mtd: device 0 fails gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
MEMERASE (0x40000 - 0x40000)
mtdgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
mtd: device 0 fails MEMERASE (0xgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
80000 - 0x40000)
mtd: Failed to gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
erase block @0x80000
mtd: devicegpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
0 fails MEMERASE (0xc0000 - 0x40gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
000)
mtd: Failed to erase block gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
@0xc0000
mtd: device 0 fails MEMgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
ERASE (0x100000 - 0x40000)
mtd: gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
Failed to erase block @0x100000
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
mtd: device 0 fails MEMERASE (0x1gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
40000 - 0x40000)
mtd: Failed to gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
erase block @0x140000
mtd: devicgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
e 0 fails MEMERASE (0x180000 - 0xgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
40000)
mtd: Failed to erase blocgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
k @0x180000
mtd: device 0 fails gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
MEMERASE (0x1c0000 - 0x40000)
mtgpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
d: Failed to erase block @0x1c0000
mtd: device 0 fails MEMERASE (0x200000 - 0x40000)
mtd: Failed to erase block@0x200000
mtd: device 0 fails MEMERASE (0x240000 - 0x40000)
mtd: Failed to erase block@0x240000
mtd: device 0 fails MEMERASE (0x280000 - 0x40000)
mtd: Failed to erase block@0x280000
mtd: device 0 fails MEMERASE (0x2c0000 - 0x40000)
mtd: Failed to erase block@0x2c0000
mtd: device 0 fails MEMERASE (0x300000 - 0x40000)
mtd: Failed to erase block@0x300000
mtd: device 0 fails MEMERASE (0x340000 - 0x40000)
mtd: Failed to erase block@0x340000
mtd: device 0 fails MEMERASE (0x380000 - 0x40utp_poll: exit with status 1280
000)
mtd: Failed to erase block@0x380000
mtd: device 0 fails MEMERASE (0x3c0000 - 0x40000)
mtd: Failed to erase block@0x3c0000
mtd: device 0 fails MEMERASE (0x400000 - 0x40000)
mtd: Failed to erase block@0x400000
mtd: device 0 fails MEMERASE (0x440000 - 0x40000)
mtd: Failed to erase block@0x440000
mtd: device 0 fails MEMERASE (0x480000 - 0x40000)
mtd: Failed to erase block@0x480000
mtd: device 0 fails MEMERASE (0x4c0000 - 0x40000)
mtd: Failed to erase block@0x4c0000
mtd: mtd_write_page failed
Failed to write safe page
mtd: Failed to write BS#0
FAILED to commit structures
UTP: sending Non-success to kernel for command $ kobs-ng init -x $FILE .
random: nonblocking pool is initialized
gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22gpmi-nand 1806000.gpmi-nand: Chip: 0, Error -22
Hi, wangqz2010@126.com
Have you referred the link I have shared previously?
IMX6UL-EVK Programming NAND via L4.1.15_2.0.0-ga_mfg-tools
Please go through the above given link. You need to add support for NAND in your software using "imx_v7_mfg_defconfig". In the above link it is given that how you can generate the NAND supported zImage and DTB. These files you need to copy in the mfgtool at "mfgtools/Profiles/Linux/OS Firmware/files/" path. After that you can flash with the .vbs script.
Regards,
Shivani
Which version BSP are you using? If you are using the newest BSP, you can refer to https://community.nxp.com/thread/517143