New design based on Sabrelite: DDR3 topology?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New design based on Sabrelite: DDR3 topology?

Jump to solution
1,205 Views
ThomasG1z
Contributor III

Doing a design that will be closely related to the Sabrelite, but a bit unsecure about the DDR3 solution. I would like all 4 chips to be on the primary side, to ease production, and would think that flyby topology would be best. Also I need the possibility to support the Solo too so the initial plan is to place the lower 2x16 bits at the end of the chain.

1. Does the concept seem fine?

2. If using fly-by are there any DDR3 register changes required compared to the sabrelite? I would really like to be able to boot up a board with the sabrelite uboot. So I have a known working good config. Haven't dove into the details here yet though.

comments...?

Labels (6)
Tags (3)
0 Kudos
Reply
1 Solution
839 Views
admin
Specialist II

From DavidBabin:

1. Yes, the concept seems fine. Flyby is better method with 4 chips on the primary side. Follow all guidelines in the Hardware Development Guide chap 3 (doc IMX6DQ6SDLHDG) for layout, write leveling, etc. An 8-chip flyby layout is shown; you can eliminate the 4 chips on the bottom. With the Solo option, be sure to minimize stubs.

2. Start with the DDR3 register settings for sabrelite. You may need to tweak drive strength settings to optimize your system.

 
3. Use the design checklist in Hardware Development Guide chap 2.

4. Simulate your layout.


View solution in original post

0 Kudos
Reply
3 Replies
839 Views
YixingKong
Senior Contributor IV

Thomas

Has your issue resolved by David's reply? If yes, please close the DI, otherwise please keep feeding back your statement here.

Thanks,

Yixing

0 Kudos
Reply
839 Views
ThomasG1z
Contributor III

Actually we ended up using only a 32-bit bus on our board, for various reasons, and T-point routing. Simulated and tested.

0 Kudos
Reply
840 Views
admin
Specialist II

From DavidBabin:

1. Yes, the concept seems fine. Flyby is better method with 4 chips on the primary side. Follow all guidelines in the Hardware Development Guide chap 3 (doc IMX6DQ6SDLHDG) for layout, write leveling, etc. An 8-chip flyby layout is shown; you can eliminate the 4 chips on the bottom. With the Solo option, be sure to minimize stubs.

2. Start with the DDR3 register settings for sabrelite. You may need to tweak drive strength settings to optimize your system.

 
3. Use the design checklist in Hardware Development Guide chap 2.

4. Simulate your layout.


0 Kudos
Reply