Need utility to program axf file in IMXRT1064 using MCU Link

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need utility to program axf file in IMXRT1064 using MCU Link

726 次查看
Vishwajeetlohar
Contributor I

Hi,

WE have developed an application on IMXRT1064. 

Now we need a utility to program this .axf file using MCU link on production line.

please suggest if this utility is available.

0 项奖励
回复
1 回复

688 次查看
Habib_MS
NXP Employee
NXP Employee

Hello @Vishwajeetlohar,

The utility that can help you in the production stage is the MCUxpresso Secure Provisioning Tool version 8.0, in this software there is a "Manufacturing tool" section where you can load the . Axf to several Boards at the same time, the following image shows where this tool is located:

Habib_Melchor_Santos_0-1713548664517.png

For more information about how this tool works, you can review chapter 5.7 of the document called MCUXpresso Secure Provisioning Tool User Guide v.8 which can be found in the following link:  MCUXpresso Secure Provisioning Tool | NXP Semiconductors

It is important to highlight that this tool is only available from version 8 of the MCUxpresso secure provisioning tool, so it is important that you have it.

BR

Habib.

0 项奖励
回复