Hi Team,
Greeting to all !
We have a requirement where we have to upgrade kernel on top of existing kernel.5.10 ,we need to upgrade to above it
5.15 or most probably 6.x [ Switch ]
So please could you help us on recipe modifications and steps for it for hardknott branch .
Thanks in Advance!!
Hi @jimmychan
I have doubts here
#1 . Since we are using hardknott branch that has default 5.10 so cant we upgrade the kernel version above 5.10 by updating the recipe ?
#2. Above mentioned repo link is for latest nanbield , but all our features are exists in hardknott , just our requirement is upgrade from 5.10 to above
So could you please help me with above two queries
Thanks
Sairam
Yes, you could change/modify the recipe file(.bb) of the linux-imx for the kernel upgrade.
What we recommended is the BSP that we have done the sanity check and verified. This is the kernel 6.x with the latest nanbield.