Need to switch from kernel.5.10 to above version kernel.6.x in hardknott branch for imx8qxpmek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need to switch from kernel.5.10 to above version kernel.6.x in hardknott branch for imx8qxpmek

1,388 Views
Ram2
Contributor III

Hi Team,

Greeting to all !

We have a requirement where we have to upgrade kernel on top of existing kernel.5.10 ,we need to upgrade to above it
5.15 or most probably 6.x [ Switch ]

So please could you help us on recipe modifications and steps for it for hardknott branch .

Thanks in Advance!! 


Tags (1)
0 Kudos
Reply
4 Replies

1,350 Views
Ram2
Contributor III

Hi @jimmychan 

I have doubts here
#1 . Since we are using hardknott branch that has default 5.10 so cant we upgrade the kernel version above 5.10 by updating the recipe ?
#2.  Above mentioned repo link is for latest nanbield , but all our features are exists in hardknott , just our requirement is upgrade from 5.10 to above

So could you please help me with above two queries 

Thanks 

Sairam

0 Kudos
Reply

1,336 Views
jimmychan
NXP TechSupport
NXP TechSupport

Yes, you could change/modify the recipe file(.bb) of the linux-imx for the kernel upgrade.

What we recommended is the BSP that we have done the sanity check and verified. This is the kernel 6.x with the latest nanbield.

0 Kudos
Reply

1,368 Views
Ram2
Contributor III

Hi Team,

Any update on above query requested, any one can help 

Will be much appreciated for your kind help . Since we are facing issue.

 

Thanks in Advance !!

Tags (1)
0 Kudos
Reply

1,354 Views
jimmychan
NXP TechSupport
NXP TechSupport

Why not use this:

repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-nanbield -m imx-6.6.3-1.0.0.xml

0 Kudos
Reply