Dear All,
I'm newbie to iMX6 ARM processor. Sorry about silly question.
As I want to tweak the DDR3 registers for DDR3 leveling...
I want to change the RTT register in the flash header file ( MR1 register – 0x01C)
Also I would like to understand the meaning and effect of the identifier "i" of "MXC_DCD_ITEM" macro.
Can anyone help me to understand ?
HI Titus
flash header is located in
ubootxx/board/freescale/mx6q_sabresd/flash_header.S
Identifier "i" of "MXC_DCD_ITEM" macro is used
for counting dcd header length
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks for your quick reply.
I want to change the following registers.
ODT -> 0x818 (0x021B0818)
Output drive strength -> 0x800 (0x021B0800)
Processor part, write leveling -> 0x808 (0x021B0808)
DDR part, write leveling -> 0x01C (0x021B001c
I want to update these register in "flash_headers.S" file in u-boot with the following values.
ODT -> 0x818 (0x021B0818) --> 0x0001111F
Output drive strength -> 0x800 (0x021B0800) --> 0xA139556B
Processor part, write leveling -> 0x808 (0x021B0808) --> 0x100
DDR part, write leveling -> 0x01C (0x021B001c --> 0xC4
Can you please help to change the values in that file.
/*
* Copyright (C) 2012 Freescale Semiconductor, Inc.
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License as
* published by the Free Software Foundation; either version 2 of
* the License, or (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License
* along with this program; if not, write to the Free Software
* Foundation, Inc., 59 Temple Place, Suite 330, Boston,
* MA 02111-1307 USA
*/
#include <config.h>
#include <asm/arch/mx6.h>
#ifdef CONFIG_FLASH_HEADER
#ifndef CONFIG_FLASH_HEADER_OFFSET
# error "Must define the offset of flash header"
#endif
#define CPU_2_BE_32(l) \
((((l) & 0x000000FF) << 24) | \
(((l) & 0x0000FF00) << 8) | \
(((l) & 0x00FF0000) >> 8) | \
(((l) & 0xFF000000) >> 24))
#define MXC_DCD_ITEM(i, addr, val) \
dcd_node_##i: \
.word CPU_2_BE_32(addr) ; \
.word CPU_2_BE_32(val) ; \
.section ".text.flasheader", "x"
b _start
.org CONFIG_FLASH_HEADER_OFFSET
ivt_header: .word 0x402000D1 /* Tag=0xD1, Len=0x0020, Ver=0x40 */
app_code_jump_v: .word _start
reserv1: .word 0x0
dcd_ptr: .word dcd_hdr
boot_data_ptr: .word boot_data
self_ptr: .word ivt_header
#ifdef CONFIG_SECURE_BOOT
app_code_csf: .word __hab_data
#else
app_code_csf: .word 0x0
#endif
reserv2: .word 0x0
boot_data: .word TEXT_BASE
#ifdef CONFIG_SECURE_BOOT
image_len: .word __hab_data_end - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET
#else
image_len: .word _end_of_copy - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET
#endif
plugin: .word 0x0
#if defined CONFIG_MX6DL_DDR3
#if defined CONFIG_DDR_32BIT
dcd_hdr: .word 0x40E001D2 /* Tag=0xD2, Len=59*8 + 4 + 4, Ver=0x40 */
write_dcd_cmd: .word 0x04DC01CC /* Tag=0xCC, Len=59*8 + 4, Param=0x04 */
MXC_DCD_ITEM(1, IOMUXC_BASE_ADDR + 0x774, 0x000C0000)
MXC_DCD_ITEM(2, IOMUXC_BASE_ADDR + 0x754, 0x00000000)
MXC_DCD_ITEM(3, IOMUXC_BASE_ADDR + 0x4ac, 0x00000030)
MXC_DCD_ITEM(4, IOMUXC_BASE_ADDR + 0x4b0, 0x00000030)
MXC_DCD_ITEM(5, IOMUXC_BASE_ADDR + 0x464, 0x00000030)
MXC_DCD_ITEM(6, IOMUXC_BASE_ADDR + 0x490, 0x00000030)
MXC_DCD_ITEM(7, IOMUXC_BASE_ADDR + 0x74c, 0x00000030)
MXC_DCD_ITEM(8, IOMUXC_BASE_ADDR + 0x494, 0x00000030)
MXC_DCD_ITEM(9, IOMUXC_BASE_ADDR + 0x4a0, 0x00000000)
MXC_DCD_ITEM(10, IOMUXC_BASE_ADDR + 0x4b4, 0x00000030)
MXC_DCD_ITEM(11, IOMUXC_BASE_ADDR + 0x4b8, 0x00000030)
MXC_DCD_ITEM(12, IOMUXC_BASE_ADDR + 0x76c, 0x00000030)
MXC_DCD_ITEM(13, IOMUXC_BASE_ADDR + 0x750, 0x00020000)
MXC_DCD_ITEM(14, IOMUXC_BASE_ADDR + 0x4bc, 0x00000030)
MXC_DCD_ITEM(15, IOMUXC_BASE_ADDR + 0x4c0, 0x00000030)
MXC_DCD_ITEM(16, IOMUXC_BASE_ADDR + 0x4c4, 0x00000030)
MXC_DCD_ITEM(17, IOMUXC_BASE_ADDR + 0x4c8, 0x00000030)
MXC_DCD_ITEM(18, IOMUXC_BASE_ADDR + 0x760, 0x00020000)
MXC_DCD_ITEM(19, IOMUXC_BASE_ADDR + 0x764, 0x00000030)
MXC_DCD_ITEM(20, IOMUXC_BASE_ADDR + 0x770, 0x00000030)
MXC_DCD_ITEM(21, IOMUXC_BASE_ADDR + 0x778, 0x00000030)
MXC_DCD_ITEM(22, IOMUXC_BASE_ADDR + 0x77c, 0x00000030)
MXC_DCD_ITEM(23, IOMUXC_BASE_ADDR + 0x470, 0x00000030)
MXC_DCD_ITEM(24, IOMUXC_BASE_ADDR + 0x474, 0x00000030)
MXC_DCD_ITEM(25, IOMUXC_BASE_ADDR + 0x478, 0x00000030)
MXC_DCD_ITEM(26, IOMUXC_BASE_ADDR + 0x47c, 0x00000030)
MXC_DCD_ITEM(27, MMDC_P0_BASE_ADDR + 0x800, 0xA1390003)
MXC_DCD_ITEM(28, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)
MXC_DCD_ITEM(29, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)
MXC_DCD_ITEM(30, MMDC_P0_BASE_ADDR + 0x83c, 0x42190219)
MXC_DCD_ITEM(31, MMDC_P0_BASE_ADDR + 0x840, 0x017B0177)
MXC_DCD_ITEM(32, MMDC_P0_BASE_ADDR + 0x848, 0x4B4D4E4D)
MXC_DCD_ITEM(33, MMDC_P0_BASE_ADDR + 0x850, 0x3F3E2D36)
MXC_DCD_ITEM(34, MMDC_P0_BASE_ADDR + 0x81c, 0x33333333)
MXC_DCD_ITEM(35, MMDC_P0_BASE_ADDR + 0x820, 0x33333333)
MXC_DCD_ITEM(36, MMDC_P0_BASE_ADDR + 0x824, 0x33333333)
MXC_DCD_ITEM(37, MMDC_P0_BASE_ADDR + 0x828, 0x33333333)
MXC_DCD_ITEM(38, MMDC_P0_BASE_ADDR + 0x8b8, 0x00000800)
MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x004, 0x0002002D)
MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x008, 0x00333030)
MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x00c, 0x3F435313)
MXC_DCD_ITEM(42, MMDC_P0_BASE_ADDR + 0x010, 0xB66E8B63)
MXC_DCD_ITEM(43, MMDC_P0_BASE_ADDR + 0x014, 0x01FF00DB)
MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x018, 0x00001740)
MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x01c, 0x00008000)
MXC_DCD_ITEM(46, MMDC_P0_BASE_ADDR + 0x02c, 0x000026d2)
MXC_DCD_ITEM(47, MMDC_P0_BASE_ADDR + 0x030, 0x00431023)
MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x040, 0x00000017)
MXC_DCD_ITEM(49, MMDC_P0_BASE_ADDR + 0x000, 0x83190000)
MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x01c, 0x04008032)
MXC_DCD_ITEM(51, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)
MXC_DCD_ITEM(52, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)
MXC_DCD_ITEM(53, MMDC_P0_BASE_ADDR + 0x01c, 0x05208030)
MXC_DCD_ITEM(54, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)
MXC_DCD_ITEM(55, MMDC_P0_BASE_ADDR + 0x020, 0x00005800)
MXC_DCD_ITEM(56, MMDC_P0_BASE_ADDR + 0x818, 0x00011117)
MXC_DCD_ITEM(57, MMDC_P0_BASE_ADDR + 0x004, 0x0002556d)
MXC_DCD_ITEM(58, MMDC_P0_BASE_ADDR + 0x404, 0x00011006)
MXC_DCD_ITEM(59, MMDC_P0_BASE_ADDR + 0x01c, 0x00000000)
#else /* i.MX6DL 64BIT-DDR */
dcd_hdr: .word 0x40A002D2 /* Tag=0xD2, Len=83*8 + 4 + 4, Ver=0x40 */
write_dcd_cmd: .word 0x049C02CC /* Tag=0xCC, Len=83*8 + 4, Param=0x04 */
# IOMUXC_BASE_ADDR = 0x20e0000
# DDR IO TYPE
MXC_DCD_ITEM(1, IOMUXC_BASE_ADDR + 0x774, 0x000c0000)
MXC_DCD_ITEM(2, IOMUXC_BASE_ADDR + 0x754, 0x00000000)
# Clock
MXC_DCD_ITEM(3, IOMUXC_BASE_ADDR + 0x4ac, 0x00000030)
MXC_DCD_ITEM(4, IOMUXC_BASE_ADDR + 0x4b0, 0x00000030)
# Address
MXC_DCD_ITEM(5, IOMUXC_BASE_ADDR + 0x464, 0x00000030)
MXC_DCD_ITEM(6, IOMUXC_BASE_ADDR + 0x490, 0x00000030)
MXC_DCD_ITEM(7, IOMUXC_BASE_ADDR + 0x74c, 0x00000030)
# Control
MXC_DCD_ITEM(8, IOMUXC_BASE_ADDR + 0x494, 0x00000030)
MXC_DCD_ITEM(9, IOMUXC_BASE_ADDR + 0x4a0, 0x00000000)
MXC_DCD_ITEM(10, IOMUXC_BASE_ADDR + 0x4b4, 0x00000030)
MXC_DCD_ITEM(11, IOMUXC_BASE_ADDR + 0x4b8, 0x00000030)
MXC_DCD_ITEM(12, IOMUXC_BASE_ADDR + 0x76c, 0x00000030)
# Data Strobe
MXC_DCD_ITEM(13, IOMUXC_BASE_ADDR + 0x750, 0x00020000)
MXC_DCD_ITEM(14, IOMUXC_BASE_ADDR + 0x4bc, 0x00000030)
MXC_DCD_ITEM(15, IOMUXC_BASE_ADDR + 0x4c0, 0x00000030)
MXC_DCD_ITEM(16, IOMUXC_BASE_ADDR + 0x4c4, 0x00000030)
MXC_DCD_ITEM(17, IOMUXC_BASE_ADDR + 0x4c8, 0x00000030)
MXC_DCD_ITEM(18, IOMUXC_BASE_ADDR + 0x4cc, 0x00000030)
MXC_DCD_ITEM(19, IOMUXC_BASE_ADDR + 0x4d0, 0x00000030)
MXC_DCD_ITEM(20, IOMUXC_BASE_ADDR + 0x4d4, 0x00000030)
MXC_DCD_ITEM(21, IOMUXC_BASE_ADDR + 0x4d8, 0x00000030)
MXC_DCD_ITEM(22, IOMUXC_BASE_ADDR + 0x760, 0x00020000)
MXC_DCD_ITEM(23, IOMUXC_BASE_ADDR + 0x764, 0x00000030)
MXC_DCD_ITEM(24, IOMUXC_BASE_ADDR + 0x770, 0x00000030)
MXC_DCD_ITEM(25, IOMUXC_BASE_ADDR + 0x778, 0x00000030)
MXC_DCD_ITEM(26, IOMUXC_BASE_ADDR + 0x77c, 0x00000030)
MXC_DCD_ITEM(27, IOMUXC_BASE_ADDR + 0x780, 0x00000030)
MXC_DCD_ITEM(28, IOMUXC_BASE_ADDR + 0x784, 0x00000030)
MXC_DCD_ITEM(29, IOMUXC_BASE_ADDR + 0x78c, 0x00000030)
MXC_DCD_ITEM(30, IOMUXC_BASE_ADDR + 0x748, 0x00000030)
MXC_DCD_ITEM(31, IOMUXC_BASE_ADDR + 0x470, 0x00000030)
MXC_DCD_ITEM(32, IOMUXC_BASE_ADDR + 0x474, 0x00000030)
MXC_DCD_ITEM(33, IOMUXC_BASE_ADDR + 0x478, 0x00000030)
MXC_DCD_ITEM(34, IOMUXC_BASE_ADDR + 0x47c, 0x00000030)
MXC_DCD_ITEM(35, IOMUXC_BASE_ADDR + 0x480, 0x00000030)
MXC_DCD_ITEM(36, IOMUXC_BASE_ADDR + 0x484, 0x00000030)
MXC_DCD_ITEM(37, IOMUXC_BASE_ADDR + 0x488, 0x00000030)
MXC_DCD_ITEM(38, IOMUXC_BASE_ADDR + 0x48c, 0x00000030)
# MMDC_P0_BASE_ADDR = 0x021b0000
# MMDC_P1_BASE_ADDR = 0x021b4000
# Calibrations
# ZQ
MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x800, 0xa1390003)
# write leveling
MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)
MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)
MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)
MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)
# DQS gating, read delay, write delay calibration values
# based on calibration compare of 0x00ffff00
MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x83c, 0x42480248)
MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x840, 0x0211020B)
MXC_DCD_ITEM(46, MMDC_P1_BASE_ADDR + 0x83C, 0x417F0211)
MXC_DCD_ITEM(47, MMDC_P1_BASE_ADDR + 0x840, 0x015D0166)
MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x848, 0x4B4C504D)
MXC_DCD_ITEM(49, MMDC_P1_BASE_ADDR + 0x848, 0x494C4F48)
MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x850, 0x3F3F2E31)
MXC_DCD_ITEM(51, MMDC_P1_BASE_ADDR + 0x850, 0x2B35382B)
MXC_DCD_ITEM(52, MMDC_P0_BASE_ADDR + 0x81c, 0x33333333)
MXC_DCD_ITEM(53, MMDC_P0_BASE_ADDR + 0x820, 0x33333333)
MXC_DCD_ITEM(54, MMDC_P0_BASE_ADDR + 0x824, 0x33333333)
MXC_DCD_ITEM(55, MMDC_P0_BASE_ADDR + 0x828, 0x33333333)
MXC_DCD_ITEM(56, MMDC_P1_BASE_ADDR + 0x81c, 0x33333333)
MXC_DCD_ITEM(57, MMDC_P1_BASE_ADDR + 0x820, 0x33333333)
MXC_DCD_ITEM(58, MMDC_P1_BASE_ADDR + 0x824, 0x33333333)
MXC_DCD_ITEM(59, MMDC_P1_BASE_ADDR + 0x828, 0x33333333)
MXC_DCD_ITEM(60, MMDC_P0_BASE_ADDR + 0x8b8, 0x00000800)
MXC_DCD_ITEM(61, MMDC_P1_BASE_ADDR + 0x8b8, 0x00000800)
# MMDC init:
# in DDR3, 64-bit mode, only MMDC0 is initiated:
MXC_DCD_ITEM(62, MMDC_P0_BASE_ADDR + 0x004, 0x0002002D)
MXC_DCD_ITEM(63, MMDC_P0_BASE_ADDR + 0x008, 0x00333030)
MXC_DCD_ITEM(64, MMDC_P0_BASE_ADDR + 0x00c, 0x3F435313)
MXC_DCD_ITEM(65, MMDC_P0_BASE_ADDR + 0x010, 0xB66E8B63)
MXC_DCD_ITEM(66, MMDC_P0_BASE_ADDR + 0x014, 0x01FF00DB)
MXC_DCD_ITEM(67, MMDC_P0_BASE_ADDR + 0x018, 0x00081740)
MXC_DCD_ITEM(68, MMDC_P0_BASE_ADDR + 0x01c, 0x00008000)
MXC_DCD_ITEM(69, MMDC_P0_BASE_ADDR + 0x02c, 0x000026d2)
MXC_DCD_ITEM(70, MMDC_P0_BASE_ADDR + 0x030, 0x00431023)
MXC_DCD_ITEM(71, MMDC_P0_BASE_ADDR + 0x040, 0x00000027)
MXC_DCD_ITEM(72, MMDC_P0_BASE_ADDR + 0x000, 0x831A0000)
# Initialize 2GB DDR3 - Micron MT41J128M
MXC_DCD_ITEM(73, MMDC_P0_BASE_ADDR + 0x01c, 0x04008032)
MXC_DCD_ITEM(74, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)
MXC_DCD_ITEM(75, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)
MXC_DCD_ITEM(76, MMDC_P0_BASE_ADDR + 0x01c, 0x05208030)
MXC_DCD_ITEM(77, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)
MXC_DCD_ITEM(78, MMDC_P0_BASE_ADDR + 0x020, 0x00005800)
MXC_DCD_ITEM(79, MMDC_P0_BASE_ADDR + 0x818, 0x00011117)
MXC_DCD_ITEM(80, MMDC_P1_BASE_ADDR + 0x818, 0x00011117)
MXC_DCD_ITEM(81, MMDC_P0_BASE_ADDR + 0x004, 0x0002556d)
MXC_DCD_ITEM(82, MMDC_P1_BASE_ADDR + 0x404, 0x00011006)
MXC_DCD_ITEM(83, MMDC_P0_BASE_ADDR + 0x01c, 0x00000000)
#endif
#else /* i.MX6Q */
dcd_hdr: .word 0x40a002D2 /* Tag=0xD2, Len=83*8 + 4 + 4, Ver=0x40 */
write_dcd_cmd: .word 0x049c02CC /* Tag=0xCC, Len=83*8 + 4, Param=0x04 */
/* DCD */
MXC_DCD_ITEM(1, IOMUXC_BASE_ADDR + 0x798, 0x000C0000)
MXC_DCD_ITEM(2, IOMUXC_BASE_ADDR + 0x758, 0x00000000)
MXC_DCD_ITEM(3, IOMUXC_BASE_ADDR + 0x588, 0x00000030)
MXC_DCD_ITEM(4, IOMUXC_BASE_ADDR + 0x594, 0x00000030)
MXC_DCD_ITEM(5, IOMUXC_BASE_ADDR + 0x56c, 0x00000030)
MXC_DCD_ITEM(6, IOMUXC_BASE_ADDR + 0x578, 0x00000030)
MXC_DCD_ITEM(7, IOMUXC_BASE_ADDR + 0x74c, 0x00000030)
MXC_DCD_ITEM(8, IOMUXC_BASE_ADDR + 0x57c, 0x00000030)
MXC_DCD_ITEM(9, IOMUXC_BASE_ADDR + 0x58c, 0x00000000)
MXC_DCD_ITEM(10, IOMUXC_BASE_ADDR + 0x59c, 0x00000030)
MXC_DCD_ITEM(11, IOMUXC_BASE_ADDR + 0x5a0, 0x00000030)
MXC_DCD_ITEM(12, IOMUXC_BASE_ADDR + 0x78c, 0x00000030)
MXC_DCD_ITEM(13, IOMUXC_BASE_ADDR + 0x750, 0x00020000)
MXC_DCD_ITEM(14, IOMUXC_BASE_ADDR + 0x5a8, 0x00000030)
MXC_DCD_ITEM(15, IOMUXC_BASE_ADDR + 0x5b0, 0x00000030)
MXC_DCD_ITEM(16, IOMUXC_BASE_ADDR + 0x524, 0x00000030)
MXC_DCD_ITEM(17, IOMUXC_BASE_ADDR + 0x51c, 0x00000030)
MXC_DCD_ITEM(18, IOMUXC_BASE_ADDR + 0x518, 0x00000030)
MXC_DCD_ITEM(19, IOMUXC_BASE_ADDR + 0x50c, 0x00000030)
MXC_DCD_ITEM(20, IOMUXC_BASE_ADDR + 0x5b8, 0x00000030)
MXC_DCD_ITEM(21, IOMUXC_BASE_ADDR + 0x5c0, 0x00000030)
MXC_DCD_ITEM(22, IOMUXC_BASE_ADDR + 0x774, 0x00020000)
MXC_DCD_ITEM(23, IOMUXC_BASE_ADDR + 0x784, 0x00000030)
MXC_DCD_ITEM(24, IOMUXC_BASE_ADDR + 0x788, 0x00000030)
MXC_DCD_ITEM(25, IOMUXC_BASE_ADDR + 0x794, 0x00000030)
MXC_DCD_ITEM(26, IOMUXC_BASE_ADDR + 0x79c, 0x00000030)
MXC_DCD_ITEM(27, IOMUXC_BASE_ADDR + 0x7a0, 0x00000030)
MXC_DCD_ITEM(28, IOMUXC_BASE_ADDR + 0x7a4, 0x00000030)
MXC_DCD_ITEM(29, IOMUXC_BASE_ADDR + 0x7a8, 0x00000030)
MXC_DCD_ITEM(30, IOMUXC_BASE_ADDR + 0x748, 0x00000030)
MXC_DCD_ITEM(31, IOMUXC_BASE_ADDR + 0x5ac, 0x00000030)
MXC_DCD_ITEM(32, IOMUXC_BASE_ADDR + 0x5b4, 0x00000030)
MXC_DCD_ITEM(33, IOMUXC_BASE_ADDR + 0x528, 0x00000030)
MXC_DCD_ITEM(34, IOMUXC_BASE_ADDR + 0x520, 0x00000030)
MXC_DCD_ITEM(35, IOMUXC_BASE_ADDR + 0x514, 0x00000030)
MXC_DCD_ITEM(36, IOMUXC_BASE_ADDR + 0x510, 0x00000030)
MXC_DCD_ITEM(37, IOMUXC_BASE_ADDR + 0x5bc, 0x00000030)
MXC_DCD_ITEM(38, IOMUXC_BASE_ADDR + 0x5c4, 0x00000030)
MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x800, 0xA1390003)
MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)
MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)
MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)
MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)
MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x83c, 0x4333033F)
MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x840, 0x032C031D)
MXC_DCD_ITEM(46, MMDC_P1_BASE_ADDR + 0x83c, 0x43200332)
MXC_DCD_ITEM(47, MMDC_P1_BASE_ADDR + 0x840, 0x031A026A)
MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x848, 0x4D464746)
MXC_DCD_ITEM(49, MMDC_P1_BASE_ADDR + 0x848, 0x47453F4D)
MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x850, 0x3E434440)
MXC_DCD_ITEM(51, MMDC_P1_BASE_ADDR + 0x850, 0x47384839)
MXC_DCD_ITEM(52, MMDC_P0_BASE_ADDR + 0x81c, 0x33333333)
MXC_DCD_ITEM(53, MMDC_P0_BASE_ADDR + 0x820, 0x33333333)
MXC_DCD_ITEM(54, MMDC_P0_BASE_ADDR + 0x824, 0x33333333)
MXC_DCD_ITEM(55, MMDC_P0_BASE_ADDR + 0x828, 0x33333333)
MXC_DCD_ITEM(56, MMDC_P1_BASE_ADDR + 0x81c, 0x33333333)
MXC_DCD_ITEM(57, MMDC_P1_BASE_ADDR + 0x820, 0x33333333)
MXC_DCD_ITEM(58, MMDC_P1_BASE_ADDR + 0x824, 0x33333333)
MXC_DCD_ITEM(59, MMDC_P1_BASE_ADDR + 0x828, 0x33333333)
MXC_DCD_ITEM(60, MMDC_P0_BASE_ADDR + 0x8b8, 0x00000800)
MXC_DCD_ITEM(61, MMDC_P1_BASE_ADDR + 0x8b8, 0x00000800)
MXC_DCD_ITEM(62, MMDC_P0_BASE_ADDR + 0x004, 0x00020036)
MXC_DCD_ITEM(63, MMDC_P0_BASE_ADDR + 0x008, 0x09444040)
MXC_DCD_ITEM(64, MMDC_P0_BASE_ADDR + 0x00c, 0x555A7975)
MXC_DCD_ITEM(65, MMDC_P0_BASE_ADDR + 0x010, 0xFF538F64)
MXC_DCD_ITEM(66, MMDC_P0_BASE_ADDR + 0x014, 0x01FF00DB)
MXC_DCD_ITEM(67, MMDC_P0_BASE_ADDR + 0x018, 0x00001740)
MXC_DCD_ITEM(68, MMDC_P0_BASE_ADDR + 0x01c, 0x00008000)
MXC_DCD_ITEM(69, MMDC_P0_BASE_ADDR + 0x02c, 0x000026D2)
MXC_DCD_ITEM(70, MMDC_P0_BASE_ADDR + 0x030, 0x005A1023)
MXC_DCD_ITEM(71, MMDC_P0_BASE_ADDR + 0x040, 0x00000027)
MXC_DCD_ITEM(72, MMDC_P0_BASE_ADDR + 0x000, 0x831A0000)
MXC_DCD_ITEM(73, MMDC_P0_BASE_ADDR + 0x01c, 0x04088032)
MXC_DCD_ITEM(74, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)
MXC_DCD_ITEM(75, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)
MXC_DCD_ITEM(76, MMDC_P0_BASE_ADDR + 0x01c, 0x09408030)
MXC_DCD_ITEM(77, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)
MXC_DCD_ITEM(78, MMDC_P0_BASE_ADDR + 0x020, 0x00005800)
MXC_DCD_ITEM(79, MMDC_P0_BASE_ADDR + 0x818, 0x00011117)
MXC_DCD_ITEM(80, MMDC_P1_BASE_ADDR + 0x818, 0x00011117)
MXC_DCD_ITEM(81, MMDC_P0_BASE_ADDR + 0x004, 0x00025576)
MXC_DCD_ITEM(82, MMDC_P0_BASE_ADDR + 0x404, 0x00011006)
MXC_DCD_ITEM(83, MMDC_P0_BASE_ADDR + 0x01c, 0x00000000)
#endif
#endif
Why do we have the following different values for the same address with different "i" identifier value ?
MXC_DCD_ITEM(73, MMDC_P0_BASE_ADDR + 0x01c, 0x04088032)
MXC_DCD_ITEM(74, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)
MXC_DCD_ITEM(75, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)
MXC_DCD_ITEM(76, MMDC_P0_BASE_ADDR + 0x01c, 0x09408030)
MXC_DCD_ITEM(77, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)
change it or add lines for example for write leveling:
"# write leveling
MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F) "
Where I need to add the above line ? anywhere ? or last line of the *.S file ?
Also, that line is already available right !
Why we are using particularly "40" ?
Any "i" identifier value we can use ?
MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)
MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)
MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)
MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)
please find attached file flash_header.S
Did you change anything in this attached file ?
I'm newbie to this, sorry for the very basic questions.
Thanks for your support.