Need to install application into i.mx28 (download link for cross compiler and ltib)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need to install application into i.mx28 (download link for cross compiler and ltib)

892 Views
chetanbidap
Contributor I

Hi,

I am new to freescale product, previously I was using other vendor board.

Now I have purchased new kit i.mx28, but to run application I need couple of things:

1. Cross compiler supported

2. Ltib link (file system and kernel source)

Please let me know where can I get above things asap.

Regards,

Chetan

Labels (3)
3 Replies

614 Views
chetanbidap
Contributor I

Thank Igor and Saurabh,

-Chetan

0 Kudos

614 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chetan

for ltib versions one can look

i.MX28 Evaluation Kit|Freescale

L2.6.35_1.1.0_ER_SOURCE  : i.MX28 Linux 2.6.35 Source Code Files and documentation.

Best regards

igor

614 Views
saurabh206
Senior Contributor III

Hi Chetan,

You can use Yocto  to get Kernel and other source code.

Yocto is simple to use.

IMX28 Yocto image

I hope this helps you.

Thanks

Saurabh