Hi,
We are using MIMXRT1024CAG4B in our design and currently, we are in the process of erasing its internal flash memory. Unfortunately, we have run into the issue shown in the attached image. We would appreciate guidance on resolving this issue.
Regards,
Sowmiya
Hello Kan,
I am one of the team member. Yes, we could able to connect the core via J link.
Hi @sowmiya_a ,
Seems you are using jlink, but were you able to connect with the core via jlink as below?
Please kindly clarify.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------