Need steps to make Yocto build for IMX6 Solo based target platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need steps to make Yocto build for IMX6 Solo based target platform

1,623件の閲覧回数
adityanagal
Contributor III

Hi ,

I want to make a customized Linux using Yocto  for the IMX6 solo based target platform  and also want to enable the audio codecs in it . Could somebody please provide me the steps for generating customized Linux using yocto.

Regards ,

Aditya Nagal

ラベル(1)
0 件の賞賛
返信
1 返信

1,460件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Aditya Nagal,

You would need to start from one of the two available BSPs, either the Community BSP which is open sourced or the BSP Release (which includes more codecs so perhaps you may want to check this one).

I would keep in mind which board you would want to use. If it’s an NXP board the BSP Release will be available for this board. If it’s a third-party board they may be support on the Community BSP. If it’s a custom board would you need to configure Yocto but I would recommend starting with a similar board and making the necessary changes.

 

The Community BSP documentation and instructions to for downloading are available on the following link:

http://freescale.github.io/

The BSP Releases are available on NXP website on Downloads under IMXLINUX.

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/em...

 

Once you have setup Yocto you should be able to build the supported images and customizing them. You may find the following Yocto training interesting:

https://community.nxp.com/docs/DOC-94849

I hope this information helps!

 Regards,

0 件の賞賛
返信