Need help to locate LINEIN1_LP pin details in neither imx8 TRM nor datasheet and ADC support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help to locate LINEIN1_LP pin details in neither imx8 TRM nor datasheet and ADC support

320件の閲覧回数
titusstalin
Contributor V

Hi,

I have i.MX8 Mini Varicite board and would like to connect 0 to 3.3 voltage to behave as ADC, so that I could read SAI3 RX Data register to get the digital data for the same. Is it feasible ? or only way to interface ADC via i2c bus ?

So am checking schematics and found LINEIN1_LP pin and that's where I need to feed analog voltage.

Unable to find more details about that pin but only I can see SAI3 details.

Here I could not find LINEIN1_LP pin detail, but schematics mentioned it.

titusstalin_1-1663700580477.png

 

 

titusstalin_0-1663700358968.png

 

titusstalin_2-1663700637012.png

 

titusstalin_3-1663700717710.png

 

ラベル(2)
0 件の賞賛
1 返信

313件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

In our NXP 8mm EVK design there is no MIC, so no LINEIN1_LP you can see, here for the audio section you only need to consider the SAI3 to connect the the audio codec chip, for the LINEIN1_LP is depend on the audio codec chip you are using, the board you mentioned is the third company design, you also can directly refer to it for this section.

0 件の賞賛