Need help to get wlan0 on IMX8MINI EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help to get wlan0 on IMX8MINI EVK

799 Views
parekhkeyur30
Contributor I

Hi,

I am using currently IMX8MINI EVK. I did successfully flash image to SD card. I did build below image.

fsl-image-validation-imx. But when I boot system, I didn't see wlan0 interface.

I want to bring up wireless interface on the board. Can anyone suggest, how do bring up wifi on board?

Do I need to build any other image or do I need build custom linux and enable any parameter to get wireless interface?

Any help will be really helpful.

0 Kudos
2 Replies

698 Views
radhikasomaiya
Senior Contributor II

Hi parekhkeyur30@gmail.com ,

             

             Can you please tell us which version of BSP are you using?

             We are able to get wlan0 through 'ifconfig -a' and 'iwconfig' for fsl-image-validation-imx sdcard image (Yocto version is L4.14.98_2.0.0, host: Ubuntu 16.04) and for prebuilt also we have verified it. Please try with prebuilt from this link. 

             Let us know if any help is required.

Regards,
Radhika Somaiya.

0 Kudos

698 Views
romitchatterjee
Contributor V

Does it show up when you issues "ifconfig -a" or "iwconfig"?

0 Kudos