Hi,
Currently I'm working on supporting a LVDS screen on MX6Q/LTIB-3.0.25-4.1.0 platform.
The LDB driver works well.
The target LVDS screen is HJ070NA-13A from INNOLUX,
and the resolution is 1204x600.
But the detailed timing information about the LVDS screen,
such as the horizontal front/back porch, hsync width,
vertical front/back porch and vsync width, is missing.
The data sheet of HJ070NA-13A from Innolux does not include
the complete information.
Anyone has the experience of supporting this screen?
Or where can I get such detailed timing information?
Thanks.
Robbie
HI Robbie,
I'm sorry I have no response for you, but another question: can You tell me the details on connection LVDS?
On particular if I need to use the RXIN0-RXIN1-RXIN2 or the RXIN1-RXIN2-RXIN3 to use the LCD on 6bit configuration and iMX6Solo board.
Thanks
Stefano
Unfortunately we have never tested that LVDS screen, the only information I got for the HJ070NA display is here:
http://www.haoyuelectronics.com/service/A10-A20/DateSheet/LCD/HJ070NA-13A_Pre-SPEC%28V02%29.pdf
I think the easiest/fastest way to get the information you are looking for, would be to contact Innolux directly