Need help on timing information of LVDS screen HJ070NA-13A from Innolux

cancel
Showing results for 
Search instead for 
Did you mean: 

Need help on timing information of LVDS screen HJ070NA-13A from Innolux

363 Views
RobbieJiang
Contributor IV

Hi,

Currently I'm working on supporting a LVDS screen on MX6Q/LTIB-3.0.25-4.1.0 platform.

The LDB driver works well.

The target LVDS screen is  HJ070NA-13A from INNOLUX,

and the resolution is 1204x600.

But the detailed timing information about the LVDS screen,

such as the horizontal front/back porch, hsync width,

vertical front/back porch and vsync width, is missing.

The data sheet of HJ070NA-13A from Innolux does not include

the complete information.

Anyone has the experience of supporting this screen?

Or where can I get such detailed timing information?

Thanks.

Robbie

Labels (3)
0 Kudos
2 Replies

61 Views
stefanogaleazzi
Contributor II

HI Robbie,

I'm sorry I have no response for you, but another question: can You tell me the details on connection LVDS?
On particular if I need to use the RXIN0-RXIN1-RXIN2 or the RXIN1-RXIN2-RXIN3 to use the LCD on 6bit configuration and iMX6Solo board.

Thanks

Stefano

0 Kudos

61 Views
SergioSolis
NXP Employee
NXP Employee

Unfortunately we have never tested that LVDS screen, the only information I got for the HJ070NA display is here:

http://www.haoyuelectronics.com/service/A10-A20/DateSheet/LCD/HJ070NA-13A_Pre-SPEC%28V02%29.pdf

I think the easiest/fastest way to get the information you are looking for, would be to contact Innolux directly

0 Kudos