Need fsl-mm-codecs library with GNU EABI version 0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need fsl-mm-codecs library with GNU EABI version 0

1,856件の閲覧回数
RobbieJiang
Contributor IV

Hi,

I have been developing with i.MX27 platform.

The Multimedia Plugins/Codecs package is MX27_FULL_VPU_LINUX_FW_2.2.5.tar.gz,

with VPU firmware 2.2.5, gstreamer plugin 1.6.1.3.

The multimedia codecs library coming with this package includes

lib_avi_drm_arm9_elinux.so, lib_avi_parser_arm9_elinux.so, lib_mp4_parser_arm9_elinux.so, which are are all

Version4 EABI. 

#readelf -h lib_mp4_parser_arm9_elinux.so

ELF Header:

  Magic:   7f 45 4c 46 01 01 01 00 00 00 00 00 00 00 00 00

  Class:                             ELF32

  Data:                              2's complement, little endian

  Version:                           1 (current)

  OS/ABI:                            UNIX - System V

  ABI Version:                       0

  Type:                              DYN (Shared object file)

  Machine:                           ARM

  Version:                           0x1

  Entry point address:               0x4abc

  Start of program headers:          52 (bytes into file)

  Start of section headers:          199788 (bytes into file)

  Flags:                             0x4000002, has entry point, Version4 EABI

  Size of this header:               52 (bytes)

  Size of program headers:           32 (bytes)

  Number of program headers:         3

  Size of section headers:           40 (bytes)

  Number of section headers:         18

  Section header string table index: 15

However, the cross compiler (gcc-4.1.1-glibc-2.4-nptl-1/arm-linux/bin/arm-linux-gcc) I'm using only supports GNU EABI.

So I'm not able to build avi/mp4 demuxer plugins with this version of mm-codecs lib and MX27_FULL_VPU_LINUX_FW_2.2.5.

Or is it possible to get a fsl_linux_mx27_codecs_1.6.1_3 package compatible with GNU EABI support?

Look forward to your reply.

Robbie

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,638件の閲覧回数
LaurenPost
NXP Employee
NXP Employee

Unfortunately the i.MX27 codecs can't be repackaged under a different tool chain.  The only solution is to use the tool chain provided with the last i.MX27 Linux BSP to get through the compilation problems.

Hope that helps!

Lauren

1,638件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Or you can also use the standard Gstreamer demuxers (qtdemux for mp4 and avidemuxer for avi) instead of the binaries provided by Freescale.

Regards,

Fabio Estevam

1,638件の閲覧回数
RobbieJiang
Contributor IV

Thank you, Fabio!

I'll try it.

Regards,

Jie

0 件の賞賛
返信