I have a 1-wire temperature sensor/UUID chip in an existing design that I would like to get rid of but I am using the UUID as a serial number. Is there a chip specific UUID somewhere in the i.MX6SL? I know that there is a OCOTP space to put a unique ID for the security sub system, but I am looking for something that will not require special programming at manufacturing.
Alternatively, the iMX6SoloLite could generate a UUID (from what random source?) and write it to the OTP the first time it powers up. Any experience doing this?
Solved! Go to Solution.
The i.MX6 SL has chip specific UUID ; fuses SJC_CHALL / UNIQUE_ID
are intended for it. Please look at Table 5-7 (Fusemap Descriptions) of
IMX6SLRM, Rev. 1, 04/2013. The i.MX6 SL parts are provided with UUID - there
is no need to burn it by customers.
The i.MX6 SL has chip specific UUID ; fuses SJC_CHALL / UNIQUE_ID
are intended for it. Please look at Table 5-7 (Fusemap Descriptions) of
IMX6SLRM, Rev. 1, 04/2013. The i.MX6 SL parts are provided with UUID - there
is no need to burn it by customers.
Yuri,
When I read the SJC_CHALL / UNIQUE_ID on my WandBoard Quad, I just get zeros:
cat /proc/cpuinfo
Serial : 0000000000000000
But, it works from u-boot, so I guess there must be a kernel mod required to access this from user space?
I think it is enabled in my Yocto recipe for the kernel build, as the defconfig file contains this setting:
| \Yocto\fsl-community-bsp\sources\meta-fsl-arm\recipes-kernel\linux\linux-imx-3.0.35\mx6q\defconfig |
CONFIG_FSL_OTP=y
But, I have tried this on several different linux distros including Ubuntu, Yocto and Android and I always get just zeros.
Do you have any idea why?
Thanks, Clay
It is needed to read the fuses to get UNIQUE_ID (UUID), assuming it is not locked.
Some fuses are reflected in /sys/fsl_otp, but hardly the UUID is located there.
U-boot has "imxotp read" command
Thanks. I saw that but thought it was just a place for the customer to store a UUID at Manufacturing time, I did not know that Freescale pre-loaded it with a UUID.
Hi, Nathan
If you don't want to use the UUID in OCOTP, maybe you can try the module of Random Number Generator (RNGB), chapter 39?
Thanks. I just wanted to make sure I wasn't missing a UUID somewhere else on the chip.