Need IMX536. 4G DDR3, MT41K256M16HA-125 IT:E Script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need IMX536. 4G DDR3, MT41K256M16HA-125 IT:E Script

712 Views
yanglius
Contributor I

Hello .

i am setting up the DDR test at my board. i download the Script from the website. but it happened erreor when do frequency test.

who can send me IMX536. 4G DDR3, MT41K256M16HA-125 IT:E Script for test. it's very urgent

thanks, Yang Liu

Labels (1)
0 Kudos
Reply
1 Reply

564 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yang

please create service request and I can provide

MX53_DDR3_register_programming_aid document

Also may be useful to look at

Re: i.MX53 DDR3 stress test hangs at DDR clock 550

Lab and Test Software (2)

DDR Stress tester kit for the i.MX51 and i.MX53 (REV 1)

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply