Need Code Signing Tool V2.3.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Need Code Signing Tool V2.3.1

跳至解决方案
1,215 次查看
JimBaxter
Contributor III

Hi, we need access to an older NXP Code Signing Tool V 2.3.1 as the V2.3.2 does not work with the project source I am working with, is there a way to download  an archived version of the tool?

标签 (3)
0 项奖励
回复
1 解答
1,093 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Jim,

this tool is only provided under NDA and the old versions are stored in local repositories, you may contact your FAE or DFAE to ask for the tool and sign the NDA.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,094 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Jim,

this tool is only provided under NDA and the old versions are stored in local repositories, you may contact your FAE or DFAE to ask for the tool and sign the NDA.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复