NXP/imx-vpuwrap: test_enc_arm_elinux failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP/imx-vpuwrap: test_enc_arm_elinux failed

698 Views
fadelta37
Contributor I

Hi,

When we tried running on our IMX8MP board the test app "test_enc_arm_elinux" that is included with the imx-vpuwrap ( https://github.com/NXP/imx-vpuwrap ) it failed with the following error:

$ ./test_enc_arm_elinux -i pool_720p59_i420.yuv -w 1280 -h 720 -f 2 -n 600 -framerate 59 -o ddv_test.h264

input YUV file : pool_720p59_i420.yuv
max frame number : 600
WARNING: MaxFS violates level limit
WARNING: MaxSBPS violates level limit
VC8000E reserve core info:80000001
CallBack_EncOneFrameOK: one frame is OK , length: 37
VCEncStrmEncode: ERROR Invalid input busChromaU
Frame Num: 0, [width x height] = [1280 x 720], enc FPS: 0, total FPS: 0
Encode Failure

What can we do to make the "test_enc_arm_elinux" encode successfuly?

0 Kudos
2 Replies

487 Views
sagarmane
Contributor II

Hi @joanxie ,

Thanks for the reply.

Could you please share the URL where I can get the  /unit_tests/VPU/hantro?

0 Kudos

693 Views
joanxie
NXP TechSupport
NXP TechSupport

try to use nxp official test package, under /unit_tests/VPU/hantro

 

0 Kudos