NXP i.mx8M Mini with 8GB LPDDR4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NXP i.mx8M Mini with 8GB LPDDR4

跳至解决方案
886 次查看
richard_hu
Contributor V

Dear, Sir:

We have a custom i.mx8M Mini board.

we have validated 4GB LPDDR4 on it and it works fine.

Now we change the LPDDR4 from 4GB to 8GB. And we encounter some problems.

 

The DDR Register Programming Aid (RPA) we use is "MX8M_Mini_LPDDR4_RPA_v18.xlsx".

The NXP DDR tool we use is "mscale_ddr_tool _v3.20_setup.exe".

 

First, we follow the DRAM datasheet to set up device information for 8GB LPDDR4 in RPA.

i.mx8MM-LPDDR4_4GB.png

Then, we load the .ds file to the board via NXP DDR tool.

DDR_tool_information.png

But the information shown in NXP DDR tool is not correct.

The "total DRAM density" should be "8192MB" instead of "4096".

And the "ROW size" should be "17" instead of "16".

If we execute the stress test, the test result shows error:

DDR_tool_stress_test_error.png

 

Is there any way to make 8GB LPDDR4 work on i.mx8M Mini?

 

Thanks~!!!

 

BR,

Richard

 

 

标记 (3)
0 项奖励
1 解答
867 次查看
richard_hu
Contributor V

We get great support from local distributer FAE.

The issue is solved.

I think we can close this thread.

Thanks~!!!

在原帖中查看解决方案

0 项奖励
1 回复
868 次查看
richard_hu
Contributor V

We get great support from local distributer FAE.

The issue is solved.

I think we can close this thread.

Thanks~!!!

0 项奖励