NXP IMX6ULL 空载超温限

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP IMX6ULL 空载超温限

4,954 Views
Mr_Ma
Contributor I

目前情况:

1、自己的开发板IMX6ULL,在85℃环境温度下空载超温限(CPU温度达到105℃以上)

2、测试官方IMX6UL-C EVK板,发现出现温度未达到105℃ debug口就卡死没反应了 cpu直接挂了

问题:是否可以说明一下这个情况呢

675662b592e6280001196320.jpg675662a7b05fa50001de124a.jpg

 

Labels (2)
0 Kudos
Reply
5 Replies

4,920 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

你好,

不清楚你所用i.MX6ULL产品型号(PN#), IMX6ULL-EVK使用的芯片是商用级芯片MCIMX6Y2DVM09AB,Junction Temp(TJ) is 0 to +95(℃). 这也是TJ未超过105℃会出现调试口失效的原因。

Mike

0 Kudos
Reply

4,913 Views
Mr_Ma
Contributor I

规格:

我这边使用验证的是NXP imx6ul 的EVK它的产品型号是MCIMX6G2CVM05AB,它是工业级的

我们自己设计的核心板使用的是NXP imx6ull的芯片,它的产品型号是MCIMX6Y2CVM08AB也是工业级的

现象:

现在NXP的imx6ul EVK出现未到温限cpu就卡死,我们的6ull-s出现空载超温限现象

0 Kudos
Reply

4,900 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

你好,

IMX6UL-EVK使用的是汽车级MCIMX6G2AVM07AB,工作结温应该高达125℃,EVK板上使用的DDR3L SDRAM型号是 MT41K256M16TW-107: P,工作温度范围: -40℃~+95℃。这个应该会影响到EVK板子整体工作温度上限。

下图为IMX6UL part number nomenclature:

Hui_Ma_0-1734317600757.png

你们设计的IMX6ULL板子出现空载超温限现象,是否会存在类似IMX6UL-EVK使用器件非工业级的现象。另外,工况温度高达80℃,电路板设计中需要采用热管理设计,请参考AN4579关于IMX6系列产品散热电路设计。祝顺利。

Mike

 

0 Kudos
Reply

4,878 Views
Mr_Ma
Contributor I

您好,

目前可以确定使用的器件都是工业级的,我们目前没有单独加散热片等方式处理,另外可以问下MCIMX6Y2CVM08AB 芯片的 power dissipation吗?

0 Kudos
Reply

4,864 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

你好,

除了IMX6ULL datasheet, 可以参考AN5345 关于IMX6ULL产品能耗管理,如何优化系统设计降低芯片能耗。祝顺利。

Mike

0 Kudos
Reply