NVCC_SRTC_POW's voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVCC_SRTC_POW's voltage

546 Views
xiaobingtang
Contributor I

    Hello, I need your help.

The problem is like this. I use a LTC3589-1 as the power supply IC for iMX536. The NVCC_SRTC_POW is supplied by LTC3589-1's LDO1. Before power up of VIO_3.3V, LDO1 is 1.3V, but after Vio is powered on as 3.3V, LDO1's voltage becomes 1.87V. Disconnect the NVCC_SRTC_POW pad and LTC3589-1's LDO1, NVCC_SRTC_POW's voltage is 1.87V, and LDO1's voltage is 1.35V. It is my first time to use LTC3589-1 as a PMIC,  Is there something fault and the fault information show out through the pad?

3x for your attention.

Labels (1)
0 Kudos
2 Replies

440 Views
xiaobingtang
Contributor I

I cut off the LT3589-1's Regulator 4 through U-boot,that is to say,there is no 3.3V power on the board,then I can measure the NVCC_SRTC_POW pad's voltage is about 0.68V.

0 Kudos

440 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Xiaobing,

     According to your description, It seems that there exists leakage of electricity at a certain place on your baord , and the issue should be caused by 3.3V output from LTC3589.

     Could you tell me the following messages about your design ?

(1)Can the board normally boot ?

(2)Can SRTC normally work ?

Regards,

Weidong

0 Kudos