NOR Flash in-place execution in i.MX7D/S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NOR Flash in-place execution in i.MX7D/S

Jump to solution
1,283 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about whether i.MX7D/S can support NOR Flash in-place execution or not.

My customer plan to use i.MX7S without DDR memory.

So they need to use NOR Flash in-place execution.

However, I can get information only for i.MX6SX as below and can't get enough information for i.MX7D/S from community

https://community.nxp.com/message/884087

https://community.nxp.com/message/504052

https://community.nxp.com/message/579122

Q1.

Can i.MX7D/S support NOR Flash in-place execution as same as i.MX6SX ?

Q2.

Do you have any sample code which can test the in-place execution in MCIMX7SABRE ?

Q3.

In my understanding, when user use in-place execution, the time for boot up is longer than boot-up with DDR. 

Am I correct ?

Ko-hey

Labels (4)
0 Kudos
Reply
1 Solution
1,194 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

1. yes it can support

2. sorry I am not aware of example, in general steps are the same as i.MX6SX

3. yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,195 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

1. yes it can support

2. sorry I am not aware of example, in general steps are the same as i.MX6SX

3. yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply