NAND two chips connection to i.MX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND two chips connection to i.MX53

565件の閲覧回数
ko-hey
Senior Contributor II

Hi all

 

Let me confirm about the connection of two NAND chips to i.MX53.

I understand that i.MX53 can connect four chips and want to connect two chips.

 

Are following connection correct ?

 

206267_206267.jpgimage003.jpg

 

Add info: I referred a following thread.

https://community.nxp.com/message/328462

 

 

Ko-hey

ラベル(1)
0 件の賞賛
2 返答(返信)

454件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes connections are correct and mentioned link provides correct info

from application team.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

454件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thank you for quick reply.

Ko-hey

0 件の賞賛