NAND flashing imx51 EVK. how ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND flashing imx51 EVK. how ?

1,036件の閲覧回数
pest
Contributor I

Hi to the experts there.

  I want to flash redboot.bin to the Micron NAND chip connected to iMX51 EVK, J16 connector. And then boot from this NAND.

What are the available means to write to this NAND falsh (to its raw partition) ?

NOTE: I have the QNX OS with BSP already running from the SDcard.

I tried dd command like: dd if=redboot.bin of=dev/etfs1 (etfs1 is the raw partition of the NAND). But fails with error /dev/etfs1 : invalid argument.

Can I flash through some tool. Or is such a facility provided by QNX IDE ?

-Deepak

ラベル(1)
0 件の賞賛
返信
0 返答(返信)