Q. What are the recomended width and voltage of the NAND Flash.
A. i.MX6Q can support both 3.3V and 1.8V NAND Flash parts, so, there is no difference here. Typically, 8-bit wide NAND Flash parts are used, since 16-bit wide ones are not widespread on the market, and they are not supported by i.MX6Q.
Q. Is there an upper limit for the size of the flash regarding the comemrcially available chips.
A. There is no memory size limitation from the i.MX6Q GPMI NAND Flash controller point of view.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------