NAND BOOT fail on iMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND BOOT fail on iMX6UL

3,124件の閲覧回数
riteshpatel
Contributor II

Hi,

I am using iMX6UL in custom board design. I am booting from SLC NAND memory. MT29F8G08ABABAWP

Please see attached schematic.

I am able to write image to the NAND Flash using USB OTG1 using serial download mode.

Configured Boot configuration resistor setting to the NAND Flash boot. See below table.

  

Boot DeviceCFG1 [7]CFG1 [6]CFG1 [5]CFG1 [4]CFG1 [3]CFG1 [2]CFG1 [1]CFG1 [0]
NAND - MT29F8G08ABABA10000000
Boot DeviceCFG2 [7CFG2 [6CFG2 [5CFG2 [4CFG2 [3CFG2 [2CFG2 [1CFG2 [0
NAND - MT29F8G08ABABA00001000
Boot DeviceCFG4 [7CFG4 [6CFG4 [5CFG4 [4CFG4 [3CFG4 [2CFG4 [1CFG4 [0
NAND - MT29F8G08ABABA00000000

 

Boot mode is set to Internal boot for booting from NAND memory. But not able to Boot from NAND Flash.

Any help will be greatly appreciated.

Thanks,

Ritesh Patel.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,898件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ritesh

please verify that nand was programmed with mfg tool

using steps described on

How-To use NAND boot on i.MX6UL EVK board

for debugging one can use procedure given on

https://community.freescale.com/thread/307723

with difference that ROM address 0x000001e0 contains pointer

to internal RAM location where boot log buffer is stored.

After fail, one can connect jtag and check boot data at 0x907400.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信