My encrypted uboot image failed to boot up on imx8mm evk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

My encrypted uboot image failed to boot up on imx8mm evk

跳至解决方案
2,164 次查看
yanghongsing1
Contributor III

I am trying to build encrypted uboot image on imx8mm EVK. I followed the document of mx8m_encrypted_boot.txt. I got error message when boot from the uboot image:

I am using  <CST 3.31 folder>linux64/cst which should support encrypted boot. Could you confirm if it support encrypted function?

U-Boot SPL 2021.04-dirty (Aug 11 2021 - 17:15:21 +0800)

DDRINFO: start DRAM init

DDRINFO: DRAM rate 3000MTS

DDRINFO:ddrphy calibration done

DDRINFO: ddrmix config done

SEC0:  RNG instantiated

Normal Boot

Trying to boot from MMC1

hab fuse not enabled

 

Authenticate image from DDR location 0x401fcdc0...

"Synchronous Abort" handler, esr 0x02000000

elr: 0000000000920000 lr : 00000000007e2d58

x 0: 0000000000917e00 x 1: 0000000000000002

x 2: 0000000047e69f9a x 3: 0000000000000000

x 4: 0000000000000001 x 5: 0000000000000040

x 6: 0000000000000000 x 7: 0000000000000000

x 8: 0000000000000000 x 9: 00000000000000cc

x10: 00000000000000f0 x11: 00000000000001fe

x12: 0000000000000000 x13: 0000000000000000

x14: 00000000000000ff x15: 0000000000000020

x16: 0000000000000000 x17: 000000001ac64259

x18: 0000000000917e50 x19: 0000000000920000

x20: 0000000000917de8 x21: 00000000007fa100

x22: 00000000007fa0e8 x23: 00000000deadbeef

x24: 00000000007f1c3e x25: 0000000000000005

x26: 00000000007f1c26 x27: 0000000072000000

x28: 0000000000000000 x29: 0000000000917d60

 

Code: 8750d8cc 86c0bc2b f32510f0 bc89c292 (09247307)

Resetting CPU ...

imx-mkimage output:

========= OFFSET dump =========

Loader IMAGE:

 header_image_off          0x0

 dcd_off                              0x0

 image_off                         0x40

 csf_off                0x2d800

 spl hab block:   0x7e0fc0 0x0 0x2d800

 

Second Loader IMAGE:

 sld_header_off                0x57c00

 sld_csf_off                        0x58c20

 sld hab block:   0x401fcdc0 0x57c00 0x1020

TEE_LOAD_ADDR=0xbe000000 ATF_LOAD_ADDR=0x00920000 VERSION=v1 ./print_fit_hab.sh 0x60000 evk.dtb

0x40200000 0x5AC00  0xED8D0

0x402ED8D0 0x1484D0 0xC730

0x920000 0x154C00 0xB160

0xBE000000 0x15FD60 0x203E60

I am using procedures below to create encrypted uboot image:

cp flash.bin flash-spl-enc.bin

../linux64/bin/cst -i csf_spl_enc.txt -o csf_spl_enc.bin

cp flash-spl-enc.bin flash-spl-enc-dummy.bin

../linux64/bin/cst -i csf_spl_sign_enc.txt -o csf_spl_sign_enc.bin

dd if=csf_spl_enc.bin of=noncemac.bin bs=1 skip=2648 count=36

dd if=noncemac.bin of=csf_spl_sign_enc.bin bs=1 seek=2648 count=36

cp flash-spl-enc.bin flash-spl-fit-enc.bin

../linux64/bin/cst -i csf_fit_enc.txt -o csf_fit_enc.bin

cp flash-spl-fit-enc.bin flash-spl-fit-enc-dummy.bin

../linux64/bin/cst -i csf_fit_sign_enc.txt -o csf_fit_sign_enc.bin

dd if=csf_fit_enc.bin of=noncemac.bin bs=1 skip=2664 count=36

dd if=noncemac.bin of=csf_fit_sign_enc.bin bs=1 seek=2688 count=36

mmc list

    

  => fatload mmc 1:1 0x40400000 dek_spl.bin

  => dek_blob 0x40400000 0x40401000 128

  => fatwrite mmc 1:1 0x40401000 dek_spl_blob.bin 0x48

  => fatload mmc 1:1 0x40402000 dek_fit.bin

  => dek_blob 0x40402000 0x40403000 128

  => fatwrite mmc 1:1 0x40403000 dek_fit_blob.bin 0x48

cp flash-spl-fit-enc.bin encrypted-flash.bin

dd if=csf_spl_sign_enc.bin of=encrypted-flash.bin seek=$((0x2d800)) bs=1 conv=notrunc

$ dd if=dek_spl_blob.bin of=encrypted-flash.bin seek=$((0x2f800)) bs=1 conv=notrunc

dd if=csf_fit_sign_enc.bin of=encrypted-flash.bin seek=$((0x58c20)) bs=1 conv=notrunc

dd if=dek_fit_blob.bin of=encrypted-flash.bin seek=$((0x363bc0)) bs=1 conv=notrunc

sudo dd if=encrypted-flash.bin of=/dev/sde bs=1K seek=33 && sync

 

Here attached all the CSF files

 

标签 (1)
0 项奖励
回复
1 解答
2,159 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hong

 

also one can try to follow AN12056  Encrypted Boot on HABv4 and CAAM Enabled Devices

(not fully applicable to i.MX8M Mini but can be used as reference)

Encrypted Boot on HABv4 and CAAM Enabled Devices 

 

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,457 次查看
mxing
Contributor II

I know it's been a couple of years since, but has this been resolved?  what are the root causes?   I'm having a similar issue.

Thanks,

Mike

0 项奖励
回复
2,160 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hong

 

also one can try to follow AN12056  Encrypted Boot on HABv4 and CAAM Enabled Devices

(not fully applicable to i.MX8M Mini but can be used as reference)

Encrypted Boot on HABv4 and CAAM Enabled Devices 

 

 

Best regards
igor

0 项奖励
回复