It can only work with .wmv and AVI format video files.I have installed associated BSP and multimedia SDK package of Freecale, but it still can't play MP4 movie . How to solve this problem? Thanks!
Hi Fugang,
Have you install the codec?
Best Regards
Dan
Hi,dan
I have installed the" WinCE700_MX53_SMD_11.05.03_ER_MM "package .Is that enough? what should I do?
Best Regards
FUGANG
Hi Fugang.
Read multimedia framework User's Guide. Attention on chapter "Check BSP modification performed by the Installer". U must have includes fslmm_mx53.reg and fslmm_mx53.bib in platform reg and bib files. I have used ARD platform and had such problem. It helped.
HI Naumov
I have checked that the fslmm_mx53.reg and fslmm_mx53.bib are existing in platform reg and bib files, that is,I can find two sentences below:
#include "$(_TARGETPLATROOT)\src\Multimedia\misc\fslmm_mx53.bib" in platform.bin file
#include "$(_TARGETPLATROOT)\src\Multimedia\misc\fslmm_mx53.reg" in platform.reg file
but it still can't work.
Hope you can give me help.
Best regards.
2013-12-06
wfg_008
发件人:Sergey Naumov <admin@community.freescale.com>
发送时间:2013-12-06 20:30
主题:Re: - My IMX53 TABLET Board run wince7.0 can't play .mp4 video under . Please help me!
收件人:"Wang Fugang"<wfg_008@126.com>
抄送:
My IMX53 TABLET Board run wince7.0 can't play .mp4 video under . Please help me!
reply from Sergey Naumov in i.MX Community - View the full discussion
Hi Fugang.
Read multimedia framework User's Guide. Attention on chapter "Check BSP modification performed by the Installer". U must have includes fslmm_mx53.reg and fslmm_mx53.bib in platform reg and bib files. I have used ARD platform and had such problem. It helped.
Reply to this message by replying to this email, or go to the message on Freescale Community
Start a new discussion in i.MX Community by email or at Freescale Community
Following My IMX53 TABLET Board run wince7.0 can't play .mp4 video under . Please help me! in these streams: Inbox
What player do You use?
Did You try PlayWnd.exe in Windows dir?
Did You follow user's guide document (maybe forgot some steps)?
Do You have fsl_*.dll DLLs in your OS image project release or debug dir?
Did You try play .mkv and .flac files?
What player do You use? Ans: windows video player sysgened with OS image by Platform Builder included
Did You try PlayWnd.exe in Windows dir?
Did You follow user's guide document (maybe forgot some steps)? Ans: YES, I think i have followed the UG
Do You have fsl_*.dll DLLs in your OS image project release or debug dir? Ans: Yes, i can see fsl_mp4_parser_v2_dshow.dll
Now, the player can only work with .wmv and .avi movie. I want it can play .mp4 file.
Thank you very much!
2013-12-06
wfg_008
发件人:Sergey Naumov <admin@community.freescale.com>
发送时间:2013-12-06 21:27
主题:Re: - My IMX53 TABLET Board run wince7.0 can't play .mp4 video under . Please help me!
收件人:"Wang Fugang"<wfg_008@126.com>
抄送:
My IMX53 TABLET Board run wince7.0 can't play .mp4 video under . Please help me!
reply from Sergey Naumov in i.MX Community - View the full discussion
What player do You use?
Did You try PlayWnd.exe in Windows dir?
Did You follow user's guide document (maybe forgot some steps)?
Do You have fsl_*.dll DLLs in your OS image project release or debug dir?
Reply to this message by replying to this email, or go to the message on Freescale Community
Start a new discussion in i.MX Community by email or at Freescale Community
Following My IMX53 TABLET Board run wince7.0 can't play .mp4 video under . Please help me! in these streams: Inbox
Dear Fugang,
You should try PlayWnd.exe player. It is in Windows dir. If it will not work, it means some problem with .mp4 codecs on your platform.