I try having Murata 1MW module working on IMX7ULP EVK. But I cannot make it work. The problem is as follows:
I would like to follow Murata datasheets for building Yocto for IMX7ULP EVK.
The user guide is excellent. It says how the Yocto customized for Murata can be downloaded and built.
The only problem is lack of documentation for IMX7.
The entire Yocto project is built with different name for the images and dtb files.
image and dtb file list |
---|
121634816 Jun 13 21:31 core-image-base-imx7ulpevk-20190613060108.rootfs.ext4 8859 Jun 13 21:31 core-image-base-imx7ulpevk-20190613060108.rootfs.manifest 39223560 Jun 13 21:49 core-image-base-imx7ulpevk-20190613060108.rootfs.sdcard.bz2 32569715 Jun 13 21:58 core-image-base-imx7ulpevk-20190613060108.rootfs.tar.bz2 150811 Jun 13 21:31 core-image-base-imx7ulpevk-20190613060108.testdata.json 53 Jun 14 15:28 core-image-base-imx7ulpevk.ext4 -> core-image-base-imx7ulpevk-20190613060108.rootfs.ext4 57 Jun 14 15:28 core-image-base-imx7ulpevk.manifest -> core-image-base-imx7ulpevk-20190613060108.rootfs.manifest 59 Jun 14 15:28 core-image-base-imx7ulpevk.sdcard.bz2 -> core-image-base-imx7ulpevk-20190613060108.rootfs.sdcard.bz2 56 Jun 14 15:28 core-image-base-imx7ulpevk.tar.bz2 -> core-image-base-imx7ulpevk-20190613060108.rootfs.tar.bz2 55 Jun 14 15:28 core-image-base-imx7ulpevk.testdata.json -> core-image-base-imx7ulpevk-20190613060108.testdata.json 61912 Jun 13 21:31 imx7ulp_erpc_matrix_multiply_rpmsg_rtos_imxcm4.img 48 Jun 14 15:28 imx7ulp-evk.dtb -> zImage--4.9.88-r0-imx7ulp-evk-20190613060108.dtb 53 Jun 14 15:28 imx7ulp-evk-emmc.dtb -> zImage--4.9.88-r0-imx7ulp-evk-emmc-20190613060108.dtb 58 Jun 14 15:28 imx7ulp-evk-emmc-qspi.dtb -> zImage--4.9.88-r0-imx7ulp-evk-emmc-qspi-20190613060108.dtb 55 Jun 14 15:28 imx7ulp-evk-ft5416.dtb -> zImage--4.9.88-r0-imx7ulp-evk-ft5416-20190613060108.dtb 55 Jun 14 15:28 imx7ulp-evk-lpuart.dtb -> zImage--4.9.88-r0-imx7ulp-evk-lpuart-20190613060108.dtb 53 Jun 14 15:28 imx7ulp-evk-mipi.dtb -> zImage--4.9.88-r0-imx7ulp-evk-mipi-20190613060108.dtb 53 Jun 14 15:28 imx7ulp-evk-qspi.dtb -> zImage--4.9.88-r0-imx7ulp-evk-qspi-20190613060108.dtb 52 Jun 14 15:28 imx7ulp-evk-sd1.dtb -> zImage--4.9.88-r0-imx7ulp-evk-sd1-20190613060108.dtb 64 Jun 14 15:28 imx7ulp-evk-sensors-to-i2c5.dtb -> zImage--4.9.88-r0-imx7ulp-evk-sensors-to-i2c5-20190613060108.dtb 55 Jun 14 15:28 imx7ulp-evk-wm8960.dtb -> zImage--4.9.88-r0-imx7ulp-evk-wm8960-20190613060108.dtb 70077 Jun 13 21:31 imx7ulp_m4_demo.img 59060 Jun 13 21:31 imx7ulp_rpmsg_lite_pingpong_rtos.img 59212 Jun 13 21:31 imx7ulp_rpmsg_lite_str_echo_rtos.img 79703 Jun 13 21:31 imx7ulp_wireless_uart_bridge.img 623986 Jun 13 21:08 modules--4.9.88-r0-imx7ulpevk-20190613060108.tgz 48 Jun 14 15:28 modules-imx7ulpevk.tgz -> modules--4.9.88-r0-imx7ulpevk-20190613060108.tgz 24 Jun 14 15:28 u-boot.imx -> u-boot-sd-2017.03-r0.imx 24 Jun 14 15:28 u-boot-imx7ulpevk.imx -> u-boot-sd-2017.03-r0.imx 24 Jun 14 15:28 u-boot-imx7ulpevk.imx-sd -> u-boot-sd-2017.03-r0.imx 24 Jun 14 15:28 u-boot.imx-sd -> u-boot-sd-2017.03-r0.imx 465920 Jun 13 21:31 u-boot-sd-2017.03-r0.imx 47 Jun 14 15:28 zImage -> zImage--4.9.88-r0-imx7ulpevk-20190613060108.bin 6892912 Jun 13 21:08 zImage--4.9.88-r0-imx7ulpevk-20190613060108.bin 21223 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-20190613060108.dtb 21235 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-emmc-20190613060108.dtb 21695 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-emmc-qspi-20190613060108.dtb 21213 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-ft5416-20190613060108.dtb 21223 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-lpuart-20190613060108.dtb 21229 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-mipi-20190613060108.dtb 21687 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-qspi-20190613060108.dtb 21487 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-sd1-20190613060108.dtb 21415 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-sensors-to-i2c5-20190613060108.dtb 24195 Jun 13 21:08 zImage--4.9.88-r0-imx7ulp-evk-wm8960-20190613060108.dtb 47 Jun 14 15:28 zImage-imx7ulpevk.bin -> zImage--4.9.88-r0-imx7ulpevk-20190613060108.bin 48 Jun 14 15:28 zImage-imx7ulp-evk.dtb -> zImage--4.9.88-r0-imx7ulp-evk-20190613060108.dtb 53 Jun 14 15:28 zImage-imx7ulp-evk-emmc.dtb -> zImage--4.9.88-r0-imx7ulp-evk-emmc-20190613060108.dtb 58 Jun 14 15:28 zImage-imx7ulp-evk-emmc-qspi.dtb -> zImage--4.9.88-r0-imx7ulp-evk-emmc-qspi-20190613060108.dtb 55 Jun 14 15:28 zImage-imx7ulp-evk-ft5416.dtb -> zImage--4.9.88-r0-imx7ulp-evk-ft5416-20190613060108.dtb 55 Jun 14 15:28 zImage-imx7ulp-evk-lpuart.dtb -> zImage--4.9.88-r0-imx7ulp-evk-lpuart-20190613060108.dtb 53 Jun 14 15:28 zImage-imx7ulp-evk-mipi.dtb -> zImage--4.9.88-r0-imx7ulp-evk-mipi-20190613060108.dtb 53 Jun 14 15:28 zImage-imx7ulp-evk-qspi.dtb -> zImage--4.9.88-r0-imx7ulp-evk-qspi-20190613060108.dtb 52 Jun 14 15:28 zImage-imx7ulp-evk-sd1.dtb -> zImage--4.9.88-r0-imx7ulp-evk-sd1-20190613060108.dtb 64 Jun 14 15:28 zImage-imx7ulp-evk-sensors-to-i2c5.dtb -> zImage--4.9.88-r0-imx7ulp-evk-sensors-to-i2c5-20190613060108.dtb 55 Jun 14 15:28 zImage-imx7ulp-evk-wm8960.dtb -> zImage--4.9.88-r0-imx7ulp-evk-wm8960-20190613060108.dtb |
I chose image: core-image-base-imx7ulpevk-20190613060108.rootfs.sdcard.bz2
But, I am not sure which dtb file I should choose.
So, I gave it a try.
I tested all the `.dtb` files
imx7ulp-evk.dtb |
with both jumper J1 on 1-2 and 3-4.
and saved them via
setenv fdt_file PATH_TO_FILE.dtb && saveenv && boot |
None of them work. Among them
imx7ulp-evk-emmc-qspi.dtb |
keep printing
mmc0: Switching to 3.3V signalling voltage failed |
regardless of J1 jumper.
The rest show no response to
dmesg | grep wifi |
as well as failing of:
ifconfig wlan0 up |
I occasionally observe
random: crng init done |
Hello,
Unfortunately, we are unable to assist you, since the i.MX7ULP is still in pre-production and we do not have information about the product. That is the reason why there is not enough information about the product.
I recommend you to go with your DFAE. They could help you with this problem.
I apologize for the inconveniences this could give you.
Best regards,
Diego.