Murata 1MW module with IMX6ULEVK not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Murata 1MW module with IMX6ULEVK not working

624件の閲覧回数
asmaa
Contributor V

Hello All,

I am using Murata 1MW module with imx6 ultralite evaluation kit, I am able to start the bluetooth and connect it to my mobile.

I am following Murata Wi-Fi/BT Solution for i.MX Quick Start Guide (Linux) 6.0 pdf

I want to do file transfer for through put measurement to evaluate it to use it in our product

Build Configuration:
BB_VERSION = "1.36.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ulevk"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.9-rocko"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:9ed1178c87afce997d5a21cadae7461fb6bb48da"
meta-oe
meta-multimedia = "HEAD:352531015014d1957d6444d114f4451e241c4d23"
meta-freescale = "HEAD:a4158e3425a79720ddc4c02e76251d567bdceb51"
meta-freescale-3rdparty = "HEAD:a02324e27f7a7ac630dab616f46a8bad7fe2c071"
meta-freescale-distro = "HEAD:51756d1c2058139c8a21f89b86cfd8007b71b7f0"
meta-bsp
meta-sdk = "HEAD:2f76097309ceb20025af6f0dd853e0f4b641d40a"
meta-browser = "HEAD:2ae23f16309d228ec6f1a25e404b3941115083ee"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:352531015014d1957d6444d114f4451e241c4d23"
meta-qt5 = "HEAD:682ad61c071a9710e9f9d8a32ab1b5f3c14953d1"
meta-murata-wireless = "HEAD:11abc9c7079cc72f454bcd5d95c1584acf311dc1"

I followed the instruction in Bluez5 Spec present at sources/meta-fsl-bsp-release/imx/tools/readme-bluez.txt

When I reach the following step:

6) Copy a file from the board to bluetooth device using the obex transfer.

Note: both obexd and obexctl need to be run from a terminal on the board
instead of from a remote login.

a) Start obex daemon
$ /usr/libexec/bluetooth/obexd

b) On a smart phone, install an obex app such as Bluetooth File Transfer.

c) Start obexctl. Type help to show commands.
$ obexctl

it does not work, it does not connect to Bluetooth File Transfer App. Bluetooth File Transfer app gives error saying the device does not support file transfer.

Regards,

Asma

タグ(2)
0 件の賞賛
1 返信

498件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not support that Murata module. What I suggest you is to go with Murata and ask for the driver and then port it to the Kernel.

I apologize for the inconveniences this could give you.

Best regards,

Diego. 

0 件の賞賛