Multiple build with different rc.local and interface files for same machine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple build with different rc.local and interface files for same machine

735件の閲覧回数
sebastiaanlaga
Contributor I

Dear People of the NXP community.

Is it possible in Yocto to do two different build one the same machine with different rc.local (fsl-rc-local) or interface (netbase). You can easy make different interface and rc.local file for different machine by using the .bbappend. But I do not know how you make different images with different rc.local and interface file for the same machine?

Kind regards

Sebastiaan

0 件の賞賛
返信
1 返信

658件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sebastiaan,

The way to configure different images for the same machine would be similar, as in that you would need to write a new image or append an existing one. Instead of changing depending on the machine you would need to have a dedicated image or image version for each configuration. I would strongly suggest that you use different image names and customize them, as this is much easier to manage than having different versions of the same image.

I hope this helps!

Regards,

0 件の賞賛
返信