Hi all,
I want to implement multibin on SD/MMC for i.MX53 WEC7. I gone through the web page at the following address
FileNotFound*KA8OBpldIOVyJF4TQizdrAdM-RkQmOiWOHPkC3QliPneRKbGAwgwtZz3QV0inJ3TFRPiwVksHuttxNTfwA6HqNq/README.txt
But this post is for i.MX50/i.MX51 on WinCE6.0. There are some changes in the files that they have mentioned in the patch. And few files are newly added as well. I am confused with this.
Does anybody have implemented this multibin on SD/MMC on i.MX53 WEC7?
Please share the experience of implementing multibin on i.MX53.
Thanks in advance,
Seetharam
There is also iMX53 WinCE700 patch: https://community.freescale.com/thread/280663
 
Hi Qiang_FSL ,
Thanks for reply..
But I am confusing about using cfimager for flashing.
If I flash using cfimager and try to load the image, it is creating new MBR etc and will format the SD card. So image will be erased.
Solution for this ??
(EDIT: Code-wise, I have already implemented all the changes in that link)
Regards,
Keshava
Hi Keshava,
cfimager -f eboot.nb0 -d F -raw -offset 0x400
The parameter "-raw" for cfimager will only write data to target address (-offset), no MBR create or sd card format.
Thanks Qiang_FSL ,
Understood.
But before loading SD image, eboot is doing the following operations:
SDHCVerifyMultiBINMBR
SDHCCreateMultiBINMBR
(Prints on log:
Successfully created 3 partitions
Boot Partition size = 767 Kbytes, startSect = 0x2, totSect = 0x5fe.
BINFS Partition size = 32768 Kbytes, startSect = 0x600, totSect = 0x10000
File System Partition size = 3838720 Kbytes, startSect = 0x10600, totSect = 0x752600
INFO: Copying NK image to RAM address 0xa0200000
)
I'm suspecting this.
Is this OK? Or whether this will format the xip.nb0 that I have flashed??
Regards,
Keshava
Hi Keshave, the EBoot will check and create the BINFS MBR for first time boot up. If the eboot.nb0 and xip.nb0 are built from the same project, no data will be destroyed.
So you just need write the EBOOT.nb0 and XIP.nb0 to sd card target address with cfimage.exe or the MFGTool, then EBOOT will do the remained work for BINFS support.
Okay Qiang_FSL ,
I have implemented all the changes and built the image.
Flashed using below commands (refering to mfgtool source code)
cfimager -f eboot.nb0 -d F -raw -offset 0x400
cfimager -f eboot.nb0 -d F -raw -offset 0x80400
cfimager -f xip.nb0 -d F -raw -offset 0x120400
Eboot is booting properly.
But its not loading the OS image.
Below is the log.
INFO: Storing boot configuration to SDHC
INFO: Successfully stored boot configuration to SDHC
System ready!
Preparing for download...
Press [ENTER] to launch image stored in SD/MMC or [SPACE] to cancel.
Initiating image launch in 1 seconds.
0 seconds.
Launching flash image ...
-BLMenu .
INFO: Using device name: 'MX6Q65535'
INFO: Reading NK image to SDHC (please wait)...
SDImageCfg.dwNkRAMOffset = 10200000
pSectorBuf = a0200000
INFO: Inside If of BSP_SUPPORT_MULTIBIN...
Inside SDHCVerifyMultiBINMBR
SDHCVerifyMultiBINMBR -
SDHCVerifyMultiBINMBR - false
Card Capacity 3872256 (Kbytes)
SDHCCreateMultiBINMBR +
SDHCCreateMultiBINMBR memset
SDMMC_WriteSector>>
Successfully created 3 partitions
Boot Partition size = 767 Kbytes, startSect = 0x2, totSect = 0x5fe.
BINFS Partition size = 32768 Kbytes, startSect = 0x600, totSect = 0x10000
File System Partition size = 3838720 Kbytes, startSect = 0x10600, totSect = 0x752600
INFO: Copying NK image to RAM address 0xa0200000
numSectors = 512
INFO: Read is 100% complete
INFO: Copy of NK completed successfully
Either card is not eSD2.1, or boot partition is not created yet
Download successful! Jumping to image at 0x0 (physical 0x10200000)...
There it stops :smileysad:
What may be the issue? Which part of the code I can suspect?
Thanks & regards,
Keshava
Can you attach your ce.bib here?
Hi Keshava, your config.bib should be wrong, from your ce.bib, it show chain.bin was put at address 80200000 ~ 80201000, the memory address 80200000 should be the kernel code running address.
Another issue in your ce.bib, there are no files in XIPKERNEL region and there are also no binfs sdmmc drivers.
So I think you havne't merged the BINFS patch correctly.
Hi Qiang_FSL , I checked the config.bib of reference in link How to support MultiBIN(BINFS) on SDMMC for Freescale IMX5x WinCE 6.0/7.0 BSP -blog archive and merged the changes.
Still the issue is not solved. I have attached the updated ce.bib. Can you please help me on this ?
The CONFIG and MEMORY section in ce.bib seems OK now. But the build script "MakeBinfsBib.js" hasn't been run on your BSP.
Please check the file name "WINCE700\PLATFORM\iMX53_SMD\FILES\imx53_SMD-preri.proj", if your BSP name is "iMX6Q_SABREAuto", this file should be renamed to "iMX6Q_SABREAuto-preri.proj".
Another thing needs be checked, you should make sure javascript can run on your PC. To check this, you can double click the "MakeBinfsBib.js" on your PC, the information should be like JS.jpg.
By the way, I still haven't seen any files be put into XIPKERNEL region, please double check your platform.bib.
@
Hi Keshava, you'd better comapre my iMX53 SMD patch with original BSP and understand the modifications.
Your ce.bib is still far away to the multibin image.
The attached is a correct multibin ce.bib, you can find XIPKERNEL files like followed, and the binfs related SD card drivers must be in XIPKERNEL region:
nk.exe I:\PB6_WorkSpaces\iMX51-EVK-Mobility\RelDir\Freescale_i_MX51_EVK_ARMV4I_Release\oal.exe XIPKERNEL MODULE SHZ
...
; ESDHC Driver
;
binfs_esdhc.dll I:\PB6_WorkSpaces\iMX51-EVK-Mobility\RelDir\Freescale_i_MX51_EVK_ARMV4I_Release\binfs_esdhc.dll XIPKERNEL SHK
binfs_sdbus.dll I:\PB6_WorkSpaces\iMX51-EVK-Mobility\RelDir\Freescale_i_MX51_EVK_ARMV4I_Release\binfs_sdbus.dll XIPKERNEL SHK
binfs_sdmemory.dll I:\PB6_WorkSpaces\iMX51-EVK-Mobility\RelDir\Freescale_i_MX51_EVK_ARMV4I_Release\binfs_sdmemory.dll XIPKERNEL SHK
Hi Qiang_FSL ,
Thank you.. Now I'm able to get the OS image (xip.nb0) loading...
But it's crashing (data abort exception) just after the OAL, and not proceeding.
Below is the log. Any idea on this?? (I have not modified the SD driver for the multibinfs implementation still. But I don't think this is the cause of this problem.. Please advice.)
LOG:
INFO: Copy of NK completed successfully
Either card is not eSD2.1, or boot partition is not created yet
Download successful! Jumping to image at 0x0 (physical 0x10200000)...
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
BSP Clock Configuration:
OSC = 24000000 Hz
PLL1 (CPU) = 792000000 Hz
PLL2 (BUS) = 528000000 Hz
PLL3 (USBOTG) = 480000000 Hz
PLL4 (AUDIO) = 0 Hz
PLL5 (VIDEO) = 0 Hz
PLL6 (MLB) = 0 Hz
PLL7 (USBHOST) = 480000000 Hz
PLL8 (ENET) = 0 Hz
PLL1_REF = 24000000 Hz
PLL2_BURNIN = 0 Hz
PLL3_60M = 60000000 Hz
PLL3_80M = 80000000 Hz
PLL3_120M = 120000000 Hz
480M_PFD0_720M = 720000000 Hz
480M_PFD1_540M = 0 Hz
480M_PFD2_508M = 508235294 Hz
480M_PFD3_454M = 454736842 Hz
528M_PFD0_352M = 352000000 Hz
528M_PFD1_594M = 594000000 Hz
528M_PFD2_400M = 396000000 Hz
528M_PFD3_200M = 594000000 Hz
ARM = 792000000 Hz
AXI = 264000000 Hz
PERIPH = 528000000 Hz
MMDC_CH0_AXI = 528000000 Hz
MMDC_CH1_AXI = 528000000 Hz
AHB_132M = 132000000 Hz
IPG = 66000000 Hz
PERCLK = 66000000 Hz
CKIL_SYNC = 0 Hz
CKIH = 0 Hz
IPU2_HSP = 264000000 Hz
IPU1_HSP = 264000000 Hz
PCIE_AXI = 264000000 Hz
VDO_AXI = 264000000 Hz
VPU_AXI = 264000000 Hz
USDHC1 = 198000000 Hz
USDHC2 = 198000000 Hz
USDHC3 = 198000000 Hz
USDHC4 = 198000000 Hz
SSI1 = 63529411 Hz
SSI2 = 63529411 Hz
SSI3 = 63529411 Hz
CAN = 30000000 Hz
UART = 80000000 Hz
SPDIF0 = 30000000 Hz
SPDIF1 = 30000000 Hz
ESAI = 30000000 Hz
ECSPI = 60000000 Hz
ACLK_EMI_SLOW = 132000000 Hz
ACLK_EMI = 132000000 Hz
ENFC = 24000000 Hz
HSI_TX = 198000000 Hz
VIDEO_27M = 0 Hz
LDB_DI0_SERIAL = 0 Hz
LDB_DI1_SERIAL = 0 Hz
LDB_DI0_IPU = 0 Hz
LDB_DI1_IPU = 0 Hz
IPU1_DI0 = 0 Hz
IPU1_DI1 = 0 Hz
IPU2_DI0 = 0 Hz
IPU2_DI1 = 0 Hz
ASRC = 0 Hz
WRCK = 0 Hz
GPU2D_CORE = 352000000 Hz
GPU2D_AXI = 264000000 Hz
GPU3D_CORE = 528000000 Hz
GPU3D_AXI = 264000000 Hz
GPU3D_SHADER = 594000000 Hz
IPP_DI0 = 0 Hz
IPP_DI1 = 0 Hz
Windows CE Kernel for ARM (Thumb Enabled)
PL310 ID = 0x410000c7
L2 cache enabled
OEMInit: silicon rev = 0x13
BoardID = 0xffff.
pdwXIPLoc = 0x70200000
WARN: OALKitlInit: KITL Disabled
SMP support disabled
dwFshFnRsvd = 0x0
cbNKPagingPoolSize = 0x200000
pdwCurXIP = 0x80200000
dwNumXIPs = 0xea0003fe
Number of XIPs exceeds MAX
All xip's added
-OEMInit
PID:00400002 TID:00510002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
PID:00400002 TID:00510002 WARNING: SNVS was reset.
PID:00400002 TID:00510002 Exception 'Data Abort' (0x4): Thread-Id=00510002(pth=c080262c), Proc-Id=00400002(pprc=8065f5e0) 'NK.EXE', VM-active=00400002(pprc=8065f5e0) 'NK.EXE'
PID:00400002 TID:00510002 PC=effb29d8(k.coredll.dll+0x000629d8) RA=eff8e96c(k.coredll.dll+0x0003e96c) SP=c48df6b0, BVA=00000000
PID:00400002 TID:00510002 Exception 'Data Abort' (0x4): Thread-Id=00510002(pth=c080262c), Proc-Id=00400002(pprc=8065f5e0) 'NK.EXE', VM-active=00400002(pprc=8065f5e0) 'NK.EXE'
PID:00400002 TID:00510002 PC=effb29d8(k.coredll.dll+0x000629d8) RA=eff8e96c(k.coredll.dll+0x0003e96c) SP=c48dfb88, BVA=00000000
Attached the ce.bib too.
Thanks.
With regards,
Keshava
Hi Keshava, you had defined pdwXIPLoc to wrong address 0x70200000 in your config.bib, that is not needed, please remove it.
nk.exe:pdwXIPLoc 00000000 70200000 FIXUPVAR
Hi Qiang_FSL ,
Thank you for confirming this... (I added it just to test, as I saw this in one other ref BSP.)
I tested by removing this. Attached the new ce.bib.
Below is the log.
Windows CE Kernel for ARM (Thumb Enabled)
PL310 ID = 0x410000c7
L2 cache enabled
OEMInit: silicon rev = 0x13
BoardID = 0xffff.
pdwXIPLoc = 0xffffffff
WARN: OALKitlInit: KITL Disabled
SMP support disabled
dwFshFnRsvd = 0x0
cbNKPagingPoolSize = 0x0
No proper XIP return
All xip's added
-OEMInit
PID:00400002 TID:00510002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
PID:00400002 TID:00510002 WARNING: SNVS was reset.
PID:00400002 TID:00510002 Exception 'Data Abort' (0x4): Thread-Id=00510002(pth=c080262c), Proc-Id=00400002(pprc=8065f5e0) 'NK.EXE', VM-active=00400002(pprc=8065f5e0) 'NK.EXE'
PID:00400002 TID:00510002 PC=effb29d8(k.coredll.dll+0x000629d8) RA=eff8e96c(k.coredll.dll+0x0003e96c) SP=c48df6b0, BVA=00000000
PID:00400002 TID:00510002 Exception 'Data Abort' (0x4): Thread-Id=00510002(pth=c080262c), Proc-Id=00400002(pprc=8065f5e0) 'NK.EXE', VM-active=00400002(pprc=8065f5e0) 'NK.EXE'
PID:00400002 TID:00510002 PC=effb29d8(k.coredll.dll+0x000629d8) RA=eff8e96c(k.coredll.dll+0x0003e96c) SP=c48dfb88, BVA=00000000
Thanks
Regards,
Keshava
All pdwXIPLoc related codes are not needed.
Yes Qiang_FSL , Even I thought of same...
I removed this extra code in OALInit. But it is not solving the issue. Below is the log.
I will try merging the only missing implementation, i.e. SD card driver changes.
But I don't think it is causing this crash, as SD driver is not loaded still...
New log:
Windows CE Kernel for ARM (Thumb Enabled)
PL310 ID = 0x410000c7
L2 cache enabled
OEMInit: silicon rev = 0x13
BoardID = 0xffff.
WARN: OALKitlInit: KITL Disabled
SMP support disabled
-OEMInit
PID:00400002 TID:00510002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
PID:00400002 TID:00510002 Exception 'Data Abort' (0x4): Thread-Id=00510002(pth=c080262c), Proc-Id=00400002(pprc=8065f5e0) 'NK.EXE', VM-active=00400002(pprc=8065f5e0) 'NK.EXE'
PID:00400002 TID:00510002 PC=effb29d8(k.coredll.dll+0x000629d8) RA=eff8e96c(k.coredll.dll+0x0003e96c) SP=c48df6b0, BVA=00000000
PID:00400002 TID:00510002 Exception 'Data Abort' (0x4): Thread-Id=00510002(pth=c080262c), Proc-Id=00400002(pprc=8065f5e0) 'NK.EXE', VM-active=00400002(pprc=8065f5e0) 'NK.EXE'
PID:00400002 TID:00510002 PC=effb29d8(k.coredll.dll+0x000629d8) RA=eff8e96c(k.coredll.dll+0x0003e96c) SP=c48dfb88, BVA=00000000
Thanks
Regards,
Keshava