Mscale DDR Tool with 8GB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mscale DDR Tool with 8GB?

767 Views
florian_arndt
Contributor V

Hi there,

 

I'm using your latest Mscale DDR Tool (version 3.20) for RAM calibration. I have a setup with i.MX 8M Plus CPU and 8GB LPDDR4 RAM (which are supported according to the CPUs datasheet).

However, even the latest Mscale DDR Tool only supports RAM density up to 6GB. Why is that? When can we expect an updated tool which supports 8GB?

Calibration (and code generation afterwards) works fine but the stress test function does not.

 

Is there a preliminary tool version with more supported RAM density available?

 

Thanks in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

601 Views
ramachandran_di
Contributor II

Hello Team,

Any update on above topic?we are also facing the same issue with 8GB.

Thnaks

Divya

0 Kudos
Reply

761 Views
joanxie
NXP TechSupport
NXP TechSupport

I have updated in salesforce, pls check it

 

0 Kudos
Reply