Hi Guys,
I am using Synchronous lcd having resolution of :
800 x 480 pixels
i have to display image of size 720 x 400 pixels.
I am using linux framebuffer with following parameters:
xres = 720
yres = 400
virtual xres = 720
virtual yres = 400
left margin = 40
right margin = 60
upper margin = 10
lower margin = 10
hsync length = 20
vsync length = 10
pixel clock = 37037
refresh rate = 57
As lcd's size is 800x480 pixels and i have to display image of size 720x400 pixels in centre of the lcd i tried to increase left margin and also upper margin so that image should move towards centre of the lcd, but changing left and upper margin's doesn't have any impact on displayed image.
Image comes left top aligned.
Any idea, any suggestions, ..how to move visible/active area towards centre of the lcd?
best regards,
vismay