Motor Control Software on RT1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Motor Control Software on RT1064

1,575 次查看
Carlio
Contributor II

Hi there,

When I’m trying to create my SDK in MCUExpresso SDK Builder, the “Motor Control Software” is not available as an option. However, it is supported for the RT1062. Are there any differences between the two processors here that I have missed? Is the Motor Control Software not supported for RT1064, and in that case why?

标记 (2)
0 项奖励
回复
3 回复数

1,535 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Carlio,

Meanwhile, you can use any of the motor control examples found in the SDK for the RT1060 in the RT1064.

0 项奖励
回复

1,527 次查看
Carlio
Contributor II

Thank you @Alexis_A ! Will do. 

0 项奖励
回复

1,554 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Carlio,

I also think that this middleware should be able for both MCUs, let me check internally if there's a reason that this software is missing.

Best Regards,

Alexis Andalon