Modifying the mpu6050 6-axis accel/gyro driver for devicetree support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Modifying the mpu6050 6-axis accel/gyro driver for devicetree support

1,694件の閲覧回数
ivannikolaenko
Contributor IV

Hi all!

I have successfully modified mpu6050 driver (3.14.52 "Jethro" kernel) for devicetree support and would like to share it with community.

Add this entry to the i2cX node of your devicetree before use the driver (replace interrupt gpio and orientation with yours):

mpu6050: mpu6050@68 {         compatible = "inv,mpu6050";         reg = <0x68>;         orientation = <2 0 0 0 1 0 0 0 2>; /* Use values > 1 instead of -1 */         interrupt-parent = <&gpio2>;         interrupts = <30 IRQ_TYPE_LEVEL_HIGH>; };

At this moment there is a "dirty hack" with an 'orientation' parameter in the driver. It is because pdata.orientation[9] is array of signed char, but devicetree arrays not support negative values (or I don't understand how to do it).

 

I would be grateful for any comments.

Best regards.

Original Attachment has been moved to: mpu6050.patch.zip

ラベル(2)
0 返答(返信)