Modify UART1 as DTE mode for IMX6Q using Android 4.4.2 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Modify UART1 as DTE mode for IMX6Q using Android 4.4.2 BSP

714件の閲覧回数
changyuheng
Contributor II

BSP version: Android 4.4.2, kernel 3.0.35

Hello:

As title, I must be choose UART1 console debug port from DCE mode to DTE mode for my custom board,

my TX and RX and connection method as follow:

CPU            PC

TX<---------- TX

RX----------> RX

Pin difinition:

MX6Q_PAD_SD3_DAT7__UART1_TXD,

MX6Q_PAD_SD3_DAT6__UART1_RXD,

And register mapping:

#define _MX6Q_PAD_SD3_DAT6__UART1_RXD IOMUX_PAD(0x0694, 0x02AC, 1, 0x0920, 3, 0)

#define _MX6Q_PAD_SD3_DAT7__UART1_TXD IOMUX_PAD(0x0690, 0x02A8, 1, 0, 0, 0)

my modified pin definition to be DTE mode as follow:

#define _MX6Q_PAD_SD3_DAT6__UART1_RXD IOMUX_PAD(0x0694, 0x02AC, 1, 0x0920, 3, 0)

#define _MX6Q_PAD_SD3_DAT7__UART1_TXD IOMUX_PAD(0x0690, 0x02A8, 1, 0x0920, 2, 0)

but my uart1 still not work, maybe I have a wrong way to modify registers, how could I fix this issue?

thanks.

ラベル(2)
タグ(1)
0 件の賞賛
2 返答(返信)

494件の閲覧回数
changyuheng
Contributor II

It still not work when I modify as follow:

#define _MX6Q_PAD_SD3_DAT6__UART1_RXD IOMUX_PAD(0x0694, 0x02AC, 1, 0, 0, 0)

#define _MX6Q_PAD_SD3_DAT7__UART1_TXD IOMUX_PAD(0x0690, 0x02A8, 1, 0x0920, 2, 0)

thanks

0 件の賞賛

494件の閲覧回数
Yuri
NXP Employee
NXP Employee

IMX6 UART has some specific implementation features. The i.MX6 DQ Reference

Manual provides clear description about internal signals and (external) multiplexing
for them. Table in the Datasheet helps to clarify it. Also - the next thread in Community
may be helpful.


"i.MX6: What does the DTE/DCE in i.MX6's UART do and how are RTS and CTS affected
by the UARTxUFCR[DTEDCE] bit?"


  https://community.freescale.com/docs/DOC-97509

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛