Model based tool to check RT1176 with memory OSPI / Hyperam

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Model based tool to check RT1176 with memory OSPI / Hyperam

1,250 次查看
AbhishekVK
Contributor I
  1. What are all the Memory modules available on FlexIO for RT1176 in Model based tool..?
  2. We want to upgrade the QSPI flash memory to OSPI flash(MX25UM51345G) /Hyperam in our design, so we need to check the feasibility
  3. What are the available OSPI and Hyperam models available in tool? Can you also share if there are any supporting files required for simulation?
  4. What are parameters we can be validated in the Model based design tool for RT1176 to OSPI/Hyperam?
0 项奖励
回复
3 回复数

1,219 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

RT1170 FlexSPI controller can connect with OSPI/HyperRAM memory devices.

Please refer below application notes for detailed info.

AN13028  Advanced HyperRAM/PSRAM Usage on i.MX RT

AN12107  How to Enable Boot from Octal SPI Flash and SD Card

AN12108  How to Enable Boot from QSPI Flash

AN12183  How to Enable Debugging for FLEXSPI NOR Flash

Wish it helps.

Mike

0 项奖励
回复

1,195 次查看
AbhishekVK
Contributor I

HI Mike 

Thanks for the information.

We want to use both OPSI Flash and Hyperam Flash on FlexIO port1 of RT1176 using Different Chip Selects and Clock Signals. Can you please check if this feasibility is good and update if there will be any issues in implementation.

SNo RT1176 Pin AssignmentOSPI
IS25WX512M
Hyperam
S27KS0643GABHV020
1GPIO_SD_B2_04 — flexspi1.B_SCLK  CK
2GPIO_SD_B2_07 — flexspi1.A_SCLK SCLK-
3GPIO_SD_B2_06 — flexspi1.A_SS0_B CS#-
4GPIO_SD_B1_02 — flexspi1.A_SS1_B /-CS#
5GPIO_SD_B2_08 — flexspi1.A_DATA[0] SIO0DQ0
6GPIO_SD_B2_09 — flexspi1.A_DATA[1] SIO1DQ1
7GPIO_SD_B2_10 — flexspi1.A_DATA[2]SIO2DQ2
8GPIO_SD_B2_11 — flexspi1.A_DATA[3]SIO3DQ3
9GPIO_SD_B2_03 — flexspi1.B_DATA[0]SIO4DQ4
10GPIO_SD_B2_02 — flexspi1.B_DATA[1]SIO5DQ5
11GPIO_SD_B2_01 — flexspi1.B_DATA[2]SIO6DQ6
12GPIO_SD_B2_00 — flexspi1.B_DATA[3]SIO7DQ7

Regards

Abhishek

0 项奖励
回复

1,192 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Based on customer application, please use RT117x FlesSPI2 module, which supports 2x8bit bus.

More detailed info, please refer below table:

Hui_Ma_0-1693968265458.png

Wish it helps.

Mike

0 项奖励
回复